2021-09-15 10:29 PM
Hello,
I configured my FD CAN on NUCLEO STM32H53 with the function as below. I want to have two RX Buffers to receive 2 specific CAN IDs.
However, when I checked RX_BUFFER0 with
if (HAL_FDCAN_IsRxBufferMessageAvailable(&hfdcan1, FDCAN_RX_BUFFER0) > 0), I do not receive anything in the buffer even though the frames were sending on the bus.
But when I checked RX_BUFFER1 with
if (HAL_FDCAN_IsRxBufferMessageAvailable(&hfdcan1, FDCAN_RX_BUFFER1) > 0) , I see CAN frame coming in. It looks like only buffer 1 working.
Do you know what I am missing here to have two buffers receiving CAN data?
Thanks!
static void MX_FDCAN1_Init(void)
{
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_NO_BRS;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = DISABLE;
hfdcan1.Init.ProtocolException = ENABLE;
hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 8;
hfdcan1.Init.NominalTimeSeg1 = 69;
hfdcan1.Init.NominalTimeSeg2 = 10;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 4;
hfdcan1.Init.DataTimeSeg1 = 15;
hfdcan1.Init.DataTimeSeg2 = 4;
hfdcan1.Init.MessageRAMOffset = 0;
hfdcan1.Init.StdFiltersNbr = 2;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.RxFifo0ElmtsNbr = 0;
hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_64;
hfdcan1.Init.RxFifo1ElmtsNbr = 0;
hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_64;
hfdcan1.Init.RxBuffersNbr = 2;
hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_64;
hfdcan1.Init.TxEventsNbr = 0;
hfdcan1.Init.TxBuffersNbr = 0;
hfdcan1.Init.TxFifoQueueElmtsNbr = 2;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_64;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
FDCAN_FilterTypeDef sFilterConfig;
/* Configure Rx filter to receive synchronization message */
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXBUFFER;
sFilterConfig.FilterID1 = 0x73B;
sFilterConfig.RxBufferIndex = 0;
sFilterConfig.IsCalibrationMsg = 0;
HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig);
/* Configure Rx filter to receive synchronization message */
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXBUFFER;
sFilterConfig.FilterID1 = 0x73A;
sFilterConfig.RxBufferIndex = 1;
sFilterConfig.IsCalibrationMsg = 0;
HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig);
/* Configure and enable Tx Delay Compensation : TdcOffset = DataTimeSeg1*DataPrescaler */
HAL_FDCAN_ConfigTxDelayCompensation(&hfdcan1, 15, 0);
HAL_FDCAN_EnableTxDelayCompensation(&hfdcan1);
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
}
Solved! Go to Solution.
2021-09-15 11:37 PM
Hi,
I think so You should be changed filter index (sFilterConfig.FilterIndex = 0) for the next buffer Rx (sFilterConfig.FilterIndex = 1)
Best Regards,
Slawek
2021-09-15 11:37 PM
Hi,
I think so You should be changed filter index (sFilterConfig.FilterIndex = 0) for the next buffer Rx (sFilterConfig.FilterIndex = 1)
Best Regards,
Slawek
2021-09-16 7:40 AM
Hello Slawek,
Thank you. Changing FIlterIndex solved the problem. I tried to understand what this FilterIndex is for, but reading in the manual, I don't see much explanation.
Would you mind to share your knowledge what this FilterIndex logic is for?
An
2024-05-12 8:28 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.