STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

problem in generating hse

we are using UFBGA 132 for BLDC motor control with HSI clock to reduce the power consumption, we have been trying out with HSE clock by enabling PD10 to high, hereby, if we try to debug it get struck in the error handler function and the status of th...

Resolved! MBED TLS and TCP

Hi ,I need to use MBED TLS and TCP in F429ZI board. I didn't see any example codes for the same . Can anyone Please share the example code.

Resolved! Observed delay during bootup

Hi,I have two batch of boards with STM32F437 controllers.Batch1: It takes the controller 1.2seconds to come upBatch2: It takes the controller 200msec to come upBoth the hardware and the firmware are same.In the Batch1, when the power up is done it ta...

ALPHA_controller.jpg BETA_controller.jpg
sameeksh by Associate
  • 1943 Views
  • 2 replies
  • 1 kudos

Compile files into RAM file system (FileX) for webserver

I have started with the Nx_WebServer demo application which requires the web content files to be loaded onto the SD card ahead of time. I am adapting the project to use a RAM file system instead of the SD card file system. However, I am struggling to...

mbrossett by Associate III
  • 2718 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 DR register 0 when multiple SPI in use

I have two SPI buses activated SPI1 (flash memory) and SPI3 (nrf24l01) on my STM32F407. Separately, they work fine. But, if I transfer something via SPI1, SPI3 read from the register always returns 0 (and in DR register for SPI3 is also 0, BUT someti...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.