2024-06-03 4:28 AM
Hi ,
I need to use MBED TLS and TCP in F429ZI board. I didn't see any example codes for the same . Can anyone Please share the example code.
Solved! Go to Solution.
2024-06-04 10:09 AM
Hello @Sivakumarzcs128 ,
There is not an out of the box example using implementing MbedTLS and TCP so you may consider using the LwIP example as a starting point for the TCP/IP stack and then integrate MbedTLS into your project. You might need to adapt the MbedTLS configuration and examples from other STM32 platforms to suit the STM32F429ZI board.
if it helps there is already an example in github you could follow.
BR
2024-06-04 10:09 AM
Hello @Sivakumarzcs128 ,
There is not an out of the box example using implementing MbedTLS and TCP so you may consider using the LwIP example as a starting point for the TCP/IP stack and then integrate MbedTLS into your project. You might need to adapt the MbedTLS configuration and examples from other STM32 platforms to suit the STM32F429ZI board.
if it helps there is already an example in github you could follow.
BR
2024-06-04 11:57 PM
Maybe you can find some help here:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.