STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_Delay stuck SysTick not triggered, workaround for stm32f105

Hi,I have scoured the web for a solution to this problem, but I cannot find one, typically the replies are the same, but the solution is never found. I have tried every other solution you will find.I was playing around with the cube mx trying to solv...

UMP-Dan by Associate II
  • 9159 Views
  • 7 replies
  • 11 kudos

I2C master transmission with DMA not Working

Hi I'm trying to establish a communication using I2C with a MCP45HVX1 digital potentiometer device with the stm32g474-re discovery board, I'm using I2C2 module that has been configured with MX with interrupt enabled. I'm using PF0 as SDA and PC4 as S...

Vueko by Associate III
  • 2299 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H7 playback example

Is there an application or example about an "audio playback" project using the SAI interface (SAIA-SAIB) connected to a Codec ?I'm using the Nucleo NUH723ZG board. Thank you, Carlo

carloV by Associate III
  • 1618 Views
  • 1 replies
  • 0 kudos

Resolved! Hello, I am trying to set up a FDCAN communication (STD Id) at a baud rate of 250 kbit/s in STM32G473RBT . The Tx part seems to work perfectly but I have a problem at the level of the reception.

I try to just toggle a led for each received frame (STD ID).With a logic analyser I checked the Rx pin on the Rx MCU and the frames arrive well. Hence my feeling that the problem lies at the level of the callback function where the MCU never go.Than...

Resolved! ADC simultaneous measurement

ADC1_IN1ADC2_IN3ADC3_IN1 As i want to measure few signals simultaneously.can i configure by this way like ADC1, ADC2, ADC 3 or Separate channels from same ADC1

sag by Associate III
  • 3432 Views
  • 8 replies
  • 0 kudos

Need help with OV7670 connection without DCMI

Hello,I want to use a OV7670 camera module with my STM32U585CIU6, which has no support for DCMI. I've been trying to do an I2C address scan but I can't get the camera address. I'm using a custom board with 3 other modules that are properly identified...

How to implement SNMP v3 on STM32F207

Posted on March 07, 2018 at 13:45HiI need to create and SNMP agent on STM32F207 MCU with lwIP & FreeRTOS (or other if needed).Also I need to implement HTTP web server to host a small management page over the same.I'm new to this kind of application ...

Resolved! Connecting external memory with STM32H753ZIT6

Hello Team,   I need to connect following two devices with STM32H753ZIT6. 1. NAND Flash- MT29F64G08AFAA 2. RTC SRAM- DS1747WP-120IND+   Kindly review the attached schematics & let me know if any changes are required. I am little worried about write p...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.