STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM low price 4xI2C, 48 pin

Hello,I am looking for STM with the following features:- 48 pin (could be 64 pin only if BGA)- 4 I2C interfaces- 1 ADC channel- most important: lowest price possibleCould somebody suggest several P/N I could check? Adam

adams1 by Associate
  • 1091 Views
  • 1 replies
  • 0 kudos

ETH_REF_CLK (PA1) noise / crosstalk on ADC1_IN0 (PA0)?

Hello,Has anyone seen ADC noise generated by the 50 MHz RMII clock (PA1) affecting the measurement on ADC1_IN0 (PA0)? (approximately 100 codes in 4096).If so does anyone had a fix to suppress it?All other ADC channels used do not have the same level ...

###### by Senior II
  • 2812 Views
  • 5 replies
  • 0 kudos

Usage of decoupling capacitor in STM32H503KBU6

Hi,      I am currently using STM32H503KBU6 MCU (32 pins). For my project the space in PCB board is critical. I have placed a LDO, Level translator, voltage supervisor and along with their associated passives in a 10mmx16mm PCB board. Now I still nee...

bhavan_kumar_0-1719978260721.png bhavan_kumar_1-1719978267514.png

Resolved! Memory usage

Hello, how to know ram memory usage using debugger, to check where memory is used. This is without FreeRTOS or CMSISI know freeRTOS has TaskGetStackHighWaterMark() 

GauravK by Senior
  • 1297 Views
  • 1 replies
  • 0 kudos

Problem in single conversion mode in ADC

Hi, While implementing a single conversion process for the Analog-to-Digital Converter (ADC) via register-level programming, the debugging phase yields a consistent output of zero, irrespective of the input. This anomaly persists even after the ADC i...

Screenshot 2024-07-03 104049.png

Is This Safe !! DMA??

Hello all I am interfacing various peripherals on the STM42F446RE, SPI, I2C, UART etc,  and in the process i'm choosing to use the DMA controller.when configuring various 3rd party ICs some may have many registers to setup, Rather than use global arr...

JHERI by Senior
  • 1682 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.