STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L053R8T6 Stop Mode 2

Hello, I am working with my custom PCB with STM32L053R8T6. My code works just fine when I run it in debug without any stop mode (deep sleep). It enters to the RTC and button interrupts perfectly. However, when I want to make the MCU enter to sleep mo...

STM32U535 hardware CRC peripheral modbus

I want to use crc hardware peripheral in STM32U535 for checking some modbus and I copied a code from this community thanks to @Tesla DeLorean . But in my case this code seems to work only for a buffer lenght multiple of four bytes. I can't found my e...

GDC by Associate II
  • 1509 Views
  • 2 replies
  • 0 kudos

Resolved! ADC and DMA: DMA not updated after first read

Below is my main.c file. I'm wanting to scan analog pins PA0 and PA1. They work individually when not using DMA, but when I try to use DMA, the analog values are read once and then never updated after that. Any ideas?  /* USER CODE BEGIN Header */ /*...

jwade19 by Associate II
  • 12879 Views
  • 10 replies
  • 0 kudos

Interfacing ADT7420 with STM32F411 MCU

i'm interfacing ADT7420 with STM32F411. As per datasheet of ADT7420 the i2c specifications are as follows: Table 2. SCL Frequency 0 - 400 kHz SCL High Pulse Width, tHIGH 0.6 μs SCL Low Pulse Width, tLOW 1.3 μs   Therefore as per my understanding the ...

NSing.5 by Senior
  • 2238 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.