STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 UART only working with debugger

Hi,I am working with STM32g491re custom board. With UART communication our STM32 and other MCU communicating.After flashing the firmware with debugger both boards are communicating properly but once power off & on If other board sends the data stm32 ...

W25Q cannot read ID

Hello!I have a W25Q128JVIQ connected to an STM32F446RE like the following:I am trying to use QuadSPI in Dual Mode, but I am having difficulties reading ANY data, like the Device ID (ABh). This is my code:  W25Q_STATE W25Q_ReadID(u8_t *buf) { QSPI...

lagzilajcsi_0-1721665117811.png lagzilajcsi_1-1721665502488.png

ST7789 spi dma library

Hi guys,I want to do a dma with HAL library for a 1.3 inch st7798 driver display (uses stm32l476rg mcu)https://github.com/Floyd-Fish/ST7789-STM32I used the library in it works fine. but I want the screen to run faster (no scans should appear on the s...

Bicer by Associate II
  • 8169 Views
  • 4 replies
  • 1 kudos

ADC with DMA in STM32U545 MCU

I am experiencing issues with the ADC and DMA configuration. Specifically, I am encountering unexpectedly high ADC conversion time despite following the standard configuration steps. Below are the details of my setup and the problem I am facing: Prob...

itzthiru by Associate II
  • 2129 Views
  • 3 replies
  • 0 kudos

Resolved! UART communication over pogopins

I am asking a question of application rather than capabilities of MCU itself.I hope to build an handheld board that is powered by batteries and using this board update other board's settings, especially date/time configurations.This requires a parser...

MKanc.1 by Associate III
  • 3345 Views
  • 3 replies
  • 5 kudos

Resolved! STM32F303xC BOOT1 bit and voltage difference

Hi all,I am currently designing a board based around the STM32F303xC MCU, and had a few questions regarding information on the datasheet.- For boot modes, the data sheet states the following:"At startup, Boot0 pin and Boot1 option bit are used to sel...

charlesa by Associate
  • 1471 Views
  • 1 replies
  • 1 kudos

STM32H747(XI) JTAG Sensing

We have a new board that uses the STM32H747 MCU and is based on an existing, proven design.Despite being schematically identical, the MCU on the new board cannot be detected by the STLINK-V3SET programmer and STM32Cube software. For whatever reason, ...

Problem with the UpdateEvent

Hi everyone, I'm new to STM32. I'm trying to use the STM32C011x4's internal temperature sensor.I'm doing the same as the website below:https://deepbluembedded.com/stm32-internal-temperature-sensor-reading-example/#:~:text=The%20STM32%20microcontrolle...

STM32F4x TIMER ETR

Hello, I am configuring a PWM Timer and I would like it to by triggered by ETR, the PWM is a 99 period, 50 duty cycles, with auto reload enable. I would like to have the PWM to be restarted (resync in a sort) at each etr rising pulse. ETR Pulse does ...

vbesson by Senior
  • 1437 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.