STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! the circuit of STM32F429 NRST

Hi all,I'm using STM32F429BIT6。my question is: C3 is 3.3uF±10%,How do you like this circuit?When WDG reset in the MCU  STM32F429BIT6,It will lead to CMOS failure of the MCU NRST?If C3 is 2.2uF±10%,the CMOS of the MCU NRST will be OK?Thanks!NRST Circu...

NRST 3.3uF.jpg wdg Reset.png

Resolved! required flash wait states for stm32u575

Where does one find documentation on the required flash wait states for stm32u575 running at a specific frequency and voltage range?In these forums and on the internet I find a number of tables but they all seem to be for other products.  I've search...

ShawnP by Associate III
  • 1956 Views
  • 2 replies
  • 4 kudos

General info on Clock and Timers

Hi!I am new to Microcontrollers so the question could be not really exciting but I think it could help me to understand how clock and timers work.  I want to toggle the LD2 every 1 sec through a TIMER. I have set up the SysClock at 2MHz and a TIMER r...

Gatsby by Associate
  • 1623 Views
  • 2 replies
  • 2 kudos

Resolved! STM32L476 USB Hardware for custom application

Hi ST,Using the STM32L476 for a custom battery-operated application, on trying to implement the USB 2.0 through a type C receptable, I need clarity on the connections of the USB.AFAIK the VBUS sensing on PA9 should be connected through a resistor div...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.