STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Three phase dual active bridge

Hi all,I am trying to implement a dual active bridge in three phase system. You need one three phase PWM system on the primary and second three phase PWM system on the secondary. Phase shift of PWMs within primary are fixed 120 deg. Same on the secon...

adamp by Associate II
  • 5574 Views
  • 6 replies
  • 0 kudos

boot application - issue with SCB_DisableDCache

does anybody have a idea why the code is stuck at below do while loop (bold marked)?.use case: for the boot application , SCB_DisableDCache () is getting called before jumping into use aplication.__STATIC_INLINE void SCB_DisableDCache (void){ #if de...

Anand Ram by Associate III
  • 9760 Views
  • 15 replies
  • 1 kudos

Resolved! how to use UART with DMA

I am using STM32H7B0VBT6 MCU.i want to transmit data using UART with DMA in normal mode.i am using "HAL_UART_Transmit_DMA(&huart4, &UART4_array[0], UART4_ARRAY_SIZE);"it sends only once , next time it do not work. Where i am doing wrong ? am I using ...

NKann.1 by Associate III
  • 11208 Views
  • 9 replies
  • 6 kudos

Failed to use I2C DMA for STM32F072

Issue description as below:1. STM32F072+STM32CUBEMX+FREERTOS+I2C1 DMA2. I2C1 was set for rx DMA 2. I use HAL_I2C_Mem_Read_DMA() for external device memory reading and it retured HAL_OK,but no data written to DMA buffer , DMA1_Channel2_3_IRQHandler fo...

supgz_0-1723110535016.png supgz_1-1723110557778.png
supgz by Associate II
  • 1798 Views
  • 2 replies
  • 1 kudos

[STM32H750] How to Debug in SDram

I use STM32H750XBH6, Flash is 128kBytes.My Program is too big,so I Write a BootLoader to load the program into sdram ,and run it in sdram.This is the setting of my APP in keil,This way can run the program successfully , but I cannot debug APP in Keil...

Passerby_0-1723087388465.jpeg
Passerby by Associate III
  • 2232 Views
  • 4 replies
  • 1 kudos

I2C3 Slave need to re-power to work

Hi All,I am Ketan, and I am implementing own driver for STM32F4 device. I have STM32F4-DISCO Development, everything looks fine when I2C talks on-board slave device (CS43L22) but when I2C talk to external slave, which is connected thorough Jumper wir...

ketan_vd by Associate
  • 1701 Views
  • 3 replies
  • 0 kudos

Unable to read second ADC channel

Hi,I am using STM32F030 for a project where I need to trigger ADC conversion every 100us. I am running this SoC on 8MHz HSI. I am using TIM3 TRG for initiating ADC conversion every 100us. I am obtain ADC every 100us with ADC_CH5 which is set to 3V3 a...

x4ce by Associate III
  • 1934 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.