STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FDCAN interrupt not working

Hello,   I am trying to use FDCAN but for some reason interrupt is not triggering. Im using PEAK CAN to send and recieve messages. With osciloscope I can see the data being transfared to the STM board but the interrupt doesn't trigger. The speed I wa...

PPopo1_0-1721635882543.png
PPopo.1 by Senior
  • 8104 Views
  • 14 replies
  • 2 kudos

Resolved! ADC Polling for multiple channel not working

i am trying to use multiple channel on a single ADC to measure certain voltages. what i have noticed is that let say i have selected 3 channels now in configuration of cube MX i select no of conversion to 3 and as soon as i do that Ranks get added be...

Screenshot 2024-08-14 103128.png
rahul7515 by Associate III
  • 2325 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L4P5G-DK + STMod+ (MB1280) + WRL-17146

Greetings,I have STM32Cube IDE installed, created some test apps, blinking LED's, RTOS threads, mutex and so on,writing on UART2 (virtual serial) is working well as I have working output on virtual COM port using putty on serial.I want to access UART...

1.png

Resolved! Possible to disable external reset on STM32G4?

I am aware of the special bits to stop the IWDG and WWDG while the core is halted, but is there a way (option byte, SWD command, SFR, etc.) to configure an STM32G4 so that it will ignore the nRST pin being pulled low? I am particularly interested in ...

jacobq by Associate III
  • 2682 Views
  • 3 replies
  • 2 kudos

Program for flashing over FD-CAN

Hi, I have ported the Open Bootloader to the STM32G431 and has flashed it and is able to communicate with it over FD-CAN. Is there any program out there that I can use to flash programs using the bootloader over FD-CAN? maybe the CLI version of the S...

STM32C011 SPI with DMA on registers

Hello, I have been prubbing to run SPI transmission using DMA for some time now. So far I am trying to send a variable, but something is not working. Without DMA it works without any problem. Would anyone be able to help?

Resolved! Syncronous Timers

Hi,I'm running two timers on STM32F303 which do square wave output on two hardware pins. They are clocked by the 72MHz internal clock. They count down to 0 and reload from ARR register, which sets the output frequency. The two timers run perfectly sy...

DetlefS by Senior
  • 2919 Views
  • 4 replies
  • 1 kudos

STM32Cube USB Host Driver Interrupt Flood

Posted on January 30, 2016 at 17:47Hey folks, I've been working on USB host driver for MIDI, and so far I can enumerate the device and get data flowing. But as soon as the device is attached I get crazy numbers of interrupts related to IN transactio...

elmood by Associate III
  • 4792 Views
  • 7 replies
  • 0 kudos

Resolved! STM32H7A3QIY6QTR+1.8V HyperRAM

Hello STM32 Teams,   I want to use STM32H7A3QIY6QTR + 1.8V HyperRAM solution. STM32H7A3 datasheet said that 1.8V HyperRAM is supported. But I can not find any 1.8V HyperRAM solution from both stm32 community and EVAL Board.  All STM32H7A3 VDD Power p...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.