2024-08-15 1:55 AM
Can Single DMA channel be used for multiple DMA Streams?
As per Table 43. DMA1 request mapping in reference manual, Can I use Channel 6 for Stream0 (TIM5_CH3), Stream 3(TIM5_CH4), Stream 4 (TIM5_CH2).
I understand that Single stream I cannot use more than one channel. But how about using same channel with multiple streams? Is it ok?
Solved! Go to Solution.
2024-08-15 3:20 AM
> Can I use Channel 6 for Stream0 (TIM5_CH3), Stream 3(TIM5_CH4), Stream 4 (TIM5_CH2).
Yes.
In context of the 'F4 DMA, "Channel" means only the request multiplexer setting. ST chose to use a confusing terminology here.
JW
2024-08-15 2:42 AM
Also, kindly note that I would be using all three streams simultaneously.
2024-08-15 3:20 AM
> Can I use Channel 6 for Stream0 (TIM5_CH3), Stream 3(TIM5_CH4), Stream 4 (TIM5_CH2).
Yes.
In context of the 'F4 DMA, "Channel" means only the request multiplexer setting. ST chose to use a confusing terminology here.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.