STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bootloader DFU on STM32F439ZITx

Hi everyone, I'm developing a bootloader that works like this. I was inspired by the example: https://github.com/pramodk51/bootloader_for_stm32f4.  I developed this initially on Nucleo F439ZI for the test phase and I managed to implement it with the ...

memory_map.png

Resolved! Returning to STM32:: STM32U0 vs STM32L0

Bonjour, (in english below)J'ai travaillé sur un Nucleo-L053R8 de 2015 à 2019 (j'ai encore le Nucleo)Je reprends un travail analogue (réseau d'IoT basse énergie(LE) en milieu agricole, capteurs (certains nécessitant ADC), commandes, petits moteurs .....

Resolved! STM32F439 I2S double the audio frequency

Hi all,I reach out to you all to give some pointers or advice for me where to look into to solve this mystery.I set up my Nuc-STM32F439ZI eval board i2s peripheral to play my audio sine wav file.I used Audacity to generate 13KHz sine wave audio file ...

STM32F429I-Disc1 LCD BSP Issue

Hello, I'm working on a project on the STM32F429I-Disc1 development board and wanted to use the BSP to write characters to the LCD screen. I used STM32CubeMX to configure with LTDC enabled with the default parameters. Since there wasn't BSP configura...

IMG_0225.jpg

USB Device hangs on high data rate in STM32H750VB

I am reaching out to request your assistance with an issue we are encountering on the STM32H750VB microcontroller related to USB data transmission. The problem arises when operating at high data rates, specifically with external USB synchronization a...

Saagar by Associate
  • 1561 Views
  • 1 replies
  • 0 kudos

I2C read operation modification in driver

I have been working on interfacing a Realtek switch and the Realtek configuration was done by i2c bit banging. I am currently trying to change to HAL I2C and am in need of performing a read operation as shown.Here the read operation is performed such...

image.png
MSGokul by Associate II
  • 1263 Views
  • 1 replies
  • 1 kudos

ADC-DMA configuration

I have 6 channels on ADC1 and 2 channels on ADC2. I need the first two channels of ADC1 to be sampled simultaneously with the two channels of ADC2. The sampling needs to be triggered by a timer and occur twice each time the timer triggers. Here’s wha...

johnjones by Associate II
  • 1599 Views
  • 1 replies
  • 0 kudos

STM32H745 SAI mono_mode

Hello community.I am having an issue with the SAI on the STM32H745 not working in mono mode.Please help me solve this problem.I would like to use SAI1 in mono mode, but the code below does not work.DMA transfer does not seem to be working.hsai_BlockA...

mk3 by Associate
  • 1385 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.