STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Trouble setting up UART on STM32 using HAL library

Hello. I am trying to setup UART on my STM32 using the HAL library and without using the .ioc file for auto-configuration. I first had a test project using the .ioc file to help me setup UART and was able to transmit data. However, when I do it mysel...

Samuri by Associate II
  • 3322 Views
  • 6 replies
  • 1 kudos

Resolved! Modbus General Software

helloI have written some software for communicating with modbus nodes that are freely available.Please see them, they may be useful for you. (See links in the conversation)

Almo by Associate
  • 1327 Views
  • 2 replies
  • 2 kudos

Resolved! TFT 16bit connections

Hello Everyone  I want connect stm32F LCd controller to TFT lcd but 16 bit  because I have lack of pins . how should I connect the RGB pins of STM32 to RGB pins of the LCD ?  In case I use the LTDC contrller in 16bits , Can I use the unused pins  RGB...

Resolved! STM32 Debugging not available

I am using STM32G031J6M6 and using NRST pin as GPIO.I have been unable to connect to STM32CubeIDE, CubeProgrammer and ST-Link Utility since then, probably because I executed __WFI() in the program.CubeProgrammer error codeSTM32 target not found! If y...

watao by Associate II
  • 8640 Views
  • 13 replies
  • 11 kudos

STM32G491 FDCAN: Issue with error counters

I have been simulating errors on the bus by removing the other node (a motor controller). As expected I see a number of failed transmissions. I can see that the FDCAN peripheral signals an Active Error on the bus (presumably as a result of not gettin...

Resolved! Unable to perform multi-byte SPI; Single OK

Hello -Board - STM32 NUCLEO-L476GPeripheral board ADXL313 (16 byte data registers)Interface - SPII  can perform single byte read, combine the 2, 8 bit values and the data is correct. Yet, when I try to perform a 2 byte SPI read, it's garbage. This wo...

roger99 by Associate III
  • 5843 Views
  • 12 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.