STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 DMA UART Transfer Issues

I am using the DMA to transfer data from UART 1 (Channel 2) and UART 2 (Channel 4). Every once and awhile the data seen on UART 2 which has a lower DMA priority will be "corrupted" by the UART 1 data. I know this because when I disable UART 1 routine...

Churby by Associate II
  • 1552 Views
  • 1 replies
  • 0 kudos

THREADX TEST CASES

Hai,https://github.com/eclipse-threadx/threadx/tree/master/test/tx/regression From that link i want to try running one of the test cases from the repo. I have STM32L496zg-p board and stm32cube IDE 1.15.1 version.  I want to add threadx manually from ...

Resolved! STM32U073RBT6 using DAC with Internal Vref (2048mV)

I am using the STM32U073RBT6. I want to output DAC using the internal reference (2048mV), but the output is based on VDD_A. Can you provide a specific example of how to use it?Summary: How to output DAC using the internal reference (2048mV) to PA4 an...

pyoruya by Associate II
  • 2272 Views
  • 4 replies
  • 2 kudos

USART1 RX_DMA issue in FreeRTOS U5A5ZJQ

Hello,I have tried to set up USART1 Receive in DMA mode and with FreeRTOS. RX is GPDMA channel 0, Circular mode, Destination increment address on, burst size 16 bytes, priority Medium. Source increment off, burst 1 byte.USART1 : 115200 baudrate, 8 bi...

Metyus by Associate II
  • 1036 Views
  • 1 replies
  • 0 kudos

Resolved! scanf() can only read one character

I am trying to use scanf() in STM32H743, referring a webpage (here). More specifically, after setting up USART1 in STM32CubeMX, I add some function prototypes like:   #ifdef __GNUC__ #define PUTCHAR_PROTOTYPE int __io_putchar(int ch) #define GETCHAR_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.