STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

C++ project but unable to use C++ code

Hello, I have created a C++ project with CubeMx / CubeIDE.  It generates the code as main.c, I have seen other post about changing the file extension each time you generate code to .cpp and I have tried that but then I get an "undefined reference to ...

brohr01 by Associate III
  • 1976 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H723 I2C MEM DMA not working

Hi,On a small project I am trying to use HAL_I2C_Mem_Read_DMA and AL_I2C_Mem_Write_DMA to get and send data to INA260 and SSD1306 without success.In main i have: MPU_Config(); SCB_EnableICache(); SCB_EnableDCache(); HAL_Init(); SystemClock_Config();...

STM32U5 Delay block with OSPI in QSPI configuration

I notice the delay block doesn't seem to be configurable for the OSPI peripheral in QSPI mode. Does any one know if it is still possible to use the delay block with a QSPI clock? I've tried coding the delay block a few different ways but it doesn't s...

EvoFrank by Associate
  • 3087 Views
  • 4 replies
  • 0 kudos

USB-PD sink not working with some Ac adapters

Hi, I´m using USB-PD (with STM32G0B1CEU6) succesfully with a lot of own boards and different AC adapters. But with one adapter I don´t get the 20V despite the source has this capability. Using a PD analyzer I can see, that with the not working adapte...

AWack by Senior
  • 1884 Views
  • 1 replies
  • 0 kudos

I2C Communication Protocol

I am currently working on I2C communication with the STM32G030F6P6 microcontroller and developing a library for slave mode. I encountered an issue where, after the master transmits a command, the slave receives and processes the data, responding acco...

Resolved! STM32H5 workshop materials and voucher

Hi I attended the "STM32H5: Ultimate combination of performance, integration and affordability" on Tuesday, May 14, 2024. I have not received the material nor the voucher. Any change to get those? Regards,Antti Vähälummukka  

vahisa by Associate
  • 2206 Views
  • 3 replies
  • 0 kudos

Resolved! workshop followup STM32H5

Hello,I also attended the online "STM32H5: Ultimate combination of performance, integration and affordability" workshop on Tuesday 20th June. I've not received any email with the links to the workshop, slides and so on. Also was told to receive a fre...

Nick_Art by Associate II
  • 5518 Views
  • 9 replies
  • 6 kudos

Resolved! STM32H743 FMC LCD (SSD1963)

HiI have a question for my colleagues who use FMC to communicate with LCD. I am using CoreH7XXI with 743. The display does not respond to the data I send to it. I used Core4X9I with 429 before and everything worked. My question is whether I need to s...

USB_Device CDC_Standalone for STM32U5

Hello,I have seen that ST provides the USB_Device legacy library which uses the OTG_FS peripheral for the NUCLEO-U575ZI-Q: https://github.com/STMicroelectronics/stm32u5-classic-coremw-apps/tree/main. In my case I am using the STM32U5G9J-DK2 evaluatio...

EnaitzO by Associate II
  • 1931 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.