2023-09-24 6:44 AM - edited 2023-09-24 7:24 AM
Hi
I have a question for my colleagues who use FMC to communicate with LCD. I am using CoreH7XXI with 743. The display does not respond to the data I send to it. I used Core4X9I with 429 before and everything worked. My question is whether I need to set something else apart from FMC. I don't know if it's a faulty module or a software problem. I've been working on this problem for three days now. I use CubeIDE 1.13.2 for configuration. I still use SDRAM. Configuration is error-free. The program does not hang. I read on the forums and no one wrote about the problems I have. Could it be faulty hardware?
Solved! Go to Solution.
2023-09-25 7:10 AM
2023-09-24 7:19 AM
Hello @budzik1678
I think it will be better to write your post in English. First, because it's the official language of the community. Also, English will give your post more visibility and make it easy to understand for all ST Community members and experts.
Best regards.
II
2023-09-24 7:48 PM
It could always be faulty hardware, but it's usually a software problem.
If you can find a relevant LCD example to start from, that may be your best approach. You can also systematically debug your code, verify hardware connections, verify software on known good hardware, etc.
In particular, be aware of caching on the M7 core. I would disable caching while debugging until the code is up and running.
2023-09-25 3:30 AM - edited 2023-09-25 3:31 AM
Also, make sure the FMC are used to connect the LCD is set as Device in MPU. You may want to check the available remaps as an alternative to programming the MPU.
At any case, the basic approach to debug this is to observe the LCD signals using LA/oscilloscope.
JW
2023-09-25 6:24 AM
I don't have an oscilloscope. I cannot check whether the control signals physically appear. I tried the MPU, but it didn't help. I looked through the registers using the debugger. I checked the states of RW, RD, CS and RS. SDRAM works fine. Only the FMC part responsible for SRAM does not work. As I wrote earlier, the display works because I checked it with STM32F429. I have to buy a new integrated circuit because I have no other way to check if this one is good.
2023-09-25 7:10 AM
2024-01-08 2:23 AM - edited 2024-01-11 3:43 AM
2024-10-07 4:07 AM
I did everything on STM32CubeMX. There was an option "FMC bank mapping" in FMC settings. I didn't know what it meant and didn't change anything. I searched for a long time on forums why my display wouldn't work and someone described this problem and its solution. In the previous integrated circuit I used (STM32F429) it wasn't there, but in this one it is (STM32H743). It also involves changing addresses.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.