STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U535CETx Power Consumption Reduction

Hello there, We are designing the STM32U535 to operate in a low-power configuration. According to the datasheet, the current consumption in Run mode is 16.3 μA/MHz at 3.3 V, which is quite low. However, when measuring the actual device, even after su...

Ka_T by Associate II
  • 2430 Views
  • 4 replies
  • 1 kudos

STM32F413CH - no response from USART1 bootloader

Hi,we are facing a strange problem. We are trying to boot up into USART1 bootloader by applying the correct pattern (BOOT0, BOOT1 pins).Then communicate with the system bootloader on USART1 (in this case 4800 Baud, even parity).There is just silence ...

STM32h745 Microcontroller Not Responding

I have an STM32H745 Discovery board. The first problem I encountered was when I was creating interfaces using TouchGFX. I could upload them to the microcontroller via the application without any issues, but when I uploaded the code file through C...

motaz9898 by Associate II
  • 3106 Views
  • 7 replies
  • 0 kudos

Resolved! my Nucleo-H755ZI-Q is not programming.

I'm new to microcontrollers. I bought a Nucleo-H755ZI-Q, I connect it to my PC, I make a simple program like turning on and off a LED but the card doesn't do it. I don't know if I have to make any adjustments because it's new.

Resolved! WRITE_REG hard fault

Hallo,I'm compiling with this option   <-fpack-struct=1>Why, with this option, the instruction<WRITE_REG(hdma->Instance->CBR1, 0U);>generates hard fault? I don't understand, without changing nothing.thank you.

IVent.1 by Senior
  • 2594 Views
  • 4 replies
  • 5 kudos

LED won't blink (Timer with PWM)

Hi could somebody please help me with this: i am a beginner ,i have set the Timer_init and Gpio_init with bare Metal i'm working in STM32F429ZIT and i'm aiming to control GPIO pins PG13 and PG14 using the PWM channels with two channel each for every ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.