STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC EOC Interrupt

Posted on May 30, 2011 at 15:08The original post was too long to process during our migration. Please click on the attachment to read the original post.

blimmer by Associate II
  • 2302 Views
  • 4 replies
  • 0 kudos

DMA transfer between ext. Memory to SDIO problem

Posted on May 30, 2011 at 18:43Hi guys, I am working on a customized board with STM32F103. I am using SDIO example from library (V3.4) but modified the memory addr to external memory addr. I got problem when DMA transfer data from external memory to...

xzhang2 by Associate II
  • 1473 Views
  • 3 replies
  • 0 kudos

RTC WaitForSynchro

Posted on May 31, 2011 at 10:28hi all, I'm using a RTC (for the first time!). During the RTC_Configuration function, execution stops in RTC_WaitForSynchro() call. void RTC_Configuration(void) {   RCC_LSICmd(ENABLE);   while (RCC_GetFlagStatus(RCC_FL...

Using USB Hid to send float/double

Posted on May 29, 2011 at 22:53Hi,I just started working with Hid class to communicate via USB with STM32F103VB. I managed to send few bytes of data at once usingUserToPMABufferCopy(Send_Buffer, ENDP1_TXADDR, 5);where Send_Buffer is declared asu8 Se...

deathclaw by Associate II
  • 2547 Views
  • 4 replies
  • 0 kudos

Fixed point library

Posted on May 31, 2011 at 11:10Hi all, In my project, I am using a GPS to measure some distances, and some angles combined with a magnetometer. Therefore, I have to do a lot of floating point operations. It's dirty, it's slow, and it's taking a lot ...

Kuikui by Associate III
  • 3175 Views
  • 4 replies
  • 0 kudos

STM32F2XX Interrupts

Posted on May 30, 2011 at 20:36I have recently ported an application from the STM32F107 to the STM32F217 using the CrossWorks from Rowley tool chain.  My '107 project builds and runs correctly.  Amongst other things this project uses interrupts to m...

configuration register (stm32f107)

Posted on May 30, 2011 at 16:50hello, does anyone have already done this for GPIO? (port A, Port B, Port C, Port D and port E). a notepad will be enought. I'm programing on IAR embedded workbench (C laguage.) I need to transfert datas with USB and ...

STM32vl discovery as st-link

Posted on May 20, 2011 at 13:52Hello, I m trying to use the stm32vldiscovery board as a stand alone st-link programer, to program a stm32f207 microcontroller, through stm3220f board. As I plug the two board one to the other, before to start the debu...

weedoug18 by Associate II
  • 1713 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.