2009-09-15 9:35 AM
Problem with I2S in slave mode
2011-05-17 4:23 AM
Hello,
I want to receive data on the I2S2 port of a STM32103ZE, in slave mode. The data in PCM format, long frame sync. The data rate is 8 kHz, and the clock frequency is 256 kHz. Data are 16 bits long, and the packet frames are 32 bits long (See figure 228 of the STM32 ref. manual Rev 09, page 606). I have configured the inputs PB12 (WS), PB13 (CK) and PB15 (SD) as floating inputs. Then I have configured the I2S2 peripheral that way :Code:
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); // SPI2 Periph clock enable
I2S_InitStructure.I2S_Mode = I2S_Mode_SlaveRx; I2S_InitStructure.I2S_Standard = I2S_Standard_PCMLong; I2S_InitStructure.I2S_DataFormat = I2S_DataFormat_16bextended; I2S_InitStructure.I2S_MCLKOutput = I2S_MCLKOutput_Disable; I2S_InitStructure.I2S_AudioFreq = I2S_AudioFreq_8k; I2S_InitStructure.I2S_CPOL = SPI_CPOL_Low; I2S_Init(SPI2, &I2S_InitStructure); I2S_Cmd(SPI2, ENABLE); // Enable SPI2 But there is a problem : data are received, but they are not in sync with the WS signal. For example, if the external device sends data 0xFF00, the STM32 may receive 0x7F8, 0x7F80, 0xFF00, 0xFE00, OxF800, 0x0003, etc ... The value changes everytime the STM32 is reset. I have checked that the WS signal is correctly connected to PB12, and that the STM32 can read it (in GPIO mode). I have probably made a mistake, but where ? May be somebody will see what's wrong ? Thanks for your help !2011-05-17 4:23 AM
Hi,
1) i don't recommend you to use SPI2(I2S2) interface in slave mode. It's more buggy than I2S3(SPI2). To get a bit more detail please read last errata sheet. 2) from my own experience i will say that is important to start master (bit clock, frame) after I2S prepared and enabled for data exchange. Otherwise data could be shifted relative to the frame (WS) signal.2011-06-02 12:11 AM
I've almost the same problem on STM32F105.
In i2s2 Slave mode (receive or transmit) PCM (long or short frame sync) 16 bit data/channel, the WS is totally ignored by the chip.
2011-06-02 7:26 AM
Also in PCM Master mode Datalen=16bit,Chlen=16bit when I2SPR=ODD|140 Fs is 16khz rather than 8 (FS =I2SxCLK / [(16*2)*((2*I2SDIV)+ODD))])
72e6/(16*2*(2*140+1))=8007.1 but not 160xx
I2S bitrate is 256khz - seems to be right (I2S bitrate = number of bits per channel × number of channels × sampling audio frequency)
16*1*16000=256000
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.