cancel
Showing results for 
Search instead for 
Did you mean: 

CAN transmit status pending (STM32F105RB)

mic
Associate II
Posted on August 08, 2011 at 11:54

I wanted to run the CAN Interface of a  STM32F105RB with the examplefile of ST (Can Network). The function  CAN_TransmitStatus( CANx, 0x0) tells me that the status of transmission is pending. Do you have any idea's for this behaviour. I'm not able to send messages.

The PHY levels are 2.1 V for CAN-Low and CAN-High.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.