STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-One: STM32F4xx ADC Channels

Posted on October 18, 2011 at 03:34The data sheet for the STM32F4 series states that 24 external ADC input channels are available, but I can find only 23 in the pin assignments. ADC3_IN8 appears to be missing. The F4 reference manual (RM0090) descri...

Retarget scanf stm32 atollic

Posted on October 17, 2011 at 18:59Hi guys,I am trying to retarget scanf for USART1 of STM32 using Atollic. I think the utilized toolchain makes use of _read_r for the scanf (please verify if possible). So I need a new definition of _read_r. Any ide...

Cygwin gcc tool-chain for bare metal STM32?

Posted on October 17, 2011 at 17:06Hi all, I noticed that arm-elf-gcc, arm-elf-binutils and arm-elf-newlib are included as pre-built packages with Cygwinports. ftp://sourceware.org/pub/cygwinports/portslist.txt Can this tool-chain be used for STM32...

FreeRTOS MPU on stm32

Posted on October 07, 2011 at 10:52Hi, I am desperately trying to get the FreeRTOS MPU port running on my STM3210e-Eval Board. (Yes I am sure that my MCU has the MPU ;) ). I cannot find a working linkerscript for the GCC Toolchain. Has anyone ever...

tor by Associate
  • 1424 Views
  • 2 replies
  • 0 kudos

TotalFifoSize in STM32f107

Posted on October 17, 2011 at 17:52I have been looking at the USB OTG Libraries for the 105/7 and I've come across the variable  TotalFifoSize.  It's set to 320, when using the Full speed core.I was wondering if anyone knew if this was because of a ...

Wii Motion Plus (Cant connect)

Posted on October 17, 2011 at 00:14The original post was too long to process during our migration. Please click on the attachment to read the original post.

VCP Demo

Posted on May 05, 2011 at 11:13VCP Demo

greg_t by Associate II
  • 2395 Views
  • 5 replies
  • 0 kudos

I2C rev. 03 19 june 2007

Posted on September 30, 2011 at 20:39Hi all,does anyone know if STM32 family I2C master supports 24-bit device ID reading from an I2C slave? I have a slave compliant to I2C rev 03 standard and I need to read it's device ID. Please help, have you any...

brazov22 by Associate II
  • 2316 Views
  • 5 replies
  • 0 kudos

STMF103R8T6 SPI2 slave receive

Posted on October 13, 2011 at 17:15Hello,We are trying to send a 44 byte report over SPI from one STM32F103 to another board.  Our master sends this data out every 5ms, and our slave receives data based on an interrupt. We are experiencing an issue ...

youssef by Associate II
  • 1768 Views
  • 4 replies
  • 0 kudos

STM32F10xxx Flash over writing/programming

Posted on October 12, 2011 at 10:48Hi, I need to reset individual bits in already written word/byte in the on-chip flash (from 0x0800 0000). The problem is that according to Programming manual PM0075 (STM32F10xxx Flash memory microcontrollers) : Fla...

vv by Associate
  • 2027 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.