2011-10-17 8:52 AM
I have been looking at the USB OTG Libraries for the 105/7 and I've come across the variable TotalFifoSize. It's set to 320, when using the Full speed core.
I was wondering if anyone knew if this was because of a hardware spec, that I can't seem to find, or if it is a choice made by the libraries, and if it is a choice, what are some of the reasons one might consider when making that choice.The value is set to 320 in the file usb_core.c around line 234. snippet of usb_core.c:..... /* initialize device cfg following its address */ if (coreID == USB_OTG_FS_CORE_ID) { baseAddress = USB_OTG_FS_BASE_ADDR; pdev->cfg.coreID = USB_OTG_FS_CORE_ID; pdev->cfg.host_channels = 8 ; pdev->cfg.dev_endpoints = 4 ; pdev->cfg.TotalFifoSize = 320; /* in 32-bits */ pdev->cfg.phy_itface = USB_OTG_EMBEDDED_PHY; ....We’re moving the ST Community to a new platform to give you a better and more reliable community experience.