2011-05-05 2:13 AM
VCP Demo
2011-05-17 5:33 AM
At a guess it is using the Unique ID of the STM32 as a USB serial number. The PC will then enumerate each uniquely. Hard code an alternate, constant, serial number.
2011-05-17 5:33 AM
Same serial number to each device is not recommended way.
Rather, no serial number is better.
When two or more devices of the same serial number of the same VID/PID are connected to single PC at the same time, Windows is confused to identify the devices. It may fail on the second device. For no serial number, Windows identify them at the USB ports to which the devices are plugged in.
On the Windows side,
IgnoreHWSerNum registry setting makes Windows ignore the difference of serial number. Instead, Windows see USB port 'location'. With this setting, all your VCP devices are assigned to the same COM port number, as long as they are plugged into the same USB port.
Using a registry editor (regedit, etc),
Add IgnoreHWSerNum entry under this key,
HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\UsbFlags\
The entry name should have VID/PID of the device.
For a device VID/PID of 0xABCD/0x1234
IgnoreHWSerNumABCD1234
Set its value to 0x01 (REG_BINARY, length must be exactly one byte)
IgnoreHWSerNum is helpful for production and testing of USB devices.
Tsuneo
2011-05-17 5:33 AM
Thanks guys - this is very helpful information
2011-10-16 12:51 AM
How do I make my device to be without serial mumber ?
2011-10-16 6:51 AM
As I recall you put a zero in the iSerialNumber field, in the device descriptor
http://www.beyondlogic.org/usbnutshell/usb5.shtmlWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.