STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Delay function in ms how?

Posted on November 22, 2011 at 14:14Hi, I need a delay(uint) function for my stm32f103ze project. My IDE is KEIL with STM32 Std.Periph. v3.5.0 I found a snipped in a KEIL example but I don't understand it and I dont know if its correct. volatile un...

sam239955 by Associate II
  • 1734 Views
  • 2 replies
  • 0 kudos

USB Host HID question

Posted on November 21, 2011 at 14:27I test the USB HOST HID example with STM32F207,a keyboard is connected to USB FS port.When the program is executed, the keyboard can be recognized by STM32F207,and LCD display message:HID device:keybd,but it doesn...

weizy by Associate
  • 1294 Views
  • 2 replies
  • 0 kudos

LCD init problem

Posted on November 17, 2011 at 16:37The original post was too long to process during our migration. Please click on the attachment to read the original post.

dileptor by Associate II
  • 1135 Views
  • 1 replies
  • 0 kudos

GPIO configuration for i2c and spi

Posted on November 21, 2011 at 22:45In principle, i2c and spi interfaces need open drain connections with (data) lines connected to pull-up resistors.However, in all the sample codes of the STM32 (examples in the peripheral library), the GPIOs for t...

hate_pod by Associate
  • 4500 Views
  • 2 replies
  • 0 kudos

Acquiring audio signal using ADC

Posted on November 21, 2011 at 16:36Hi all, I am a newbiew with audio projects and I need your skills... I am acquiring the analog signal using the ADC of the STM32 and now I need a digital filter to filter out the noise. Once done I will output the...

trouble STM32F103ZET6 make reset on warm up !!!

Posted on November 21, 2011 at 22:06Hello, I have a very big problem. I have change the code and then when I make the board warm to 40�C..60�C, the processor make a reset. If I revert my change, then I can warm up the procoessor like coocing and no ...

mm by Associate II
  • 610 Views
  • 0 replies
  • 0 kudos

Full upgrade of flash

Posted on November 20, 2011 at 23:44Hej I want to write procedure that upgrades code in internal flash. It will be full upgrade of flash with executing mass erase command, so I should copy upgrade procedure to ram, execute it from ram and upgrade pr...

wadi by Associate II
  • 820 Views
  • 2 replies
  • 0 kudos

USART problem

Posted on November 10, 2011 at 10:21Hi, I wrote the code for the USART3 initialization and it does not work (cannot see anything on the scope while sending data). Can you tell me if I am doing something wrong? //configure clock for USART RCC_APB1Pe...

EXT Interrupts not happening ?

Posted on November 20, 2011 at 12:21I use the STM32F103RTE6, I cannot get the EXT interrupts to happen: I do the following: - RCC config, all the IO port clock are set RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIO_DISCONNECT|RCC_APB1Periph_TIM2|RCC_APB...

benbb by Associate II
  • 2956 Views
  • 6 replies
  • 0 kudos

TIM2 Interrupt -> HardFault Exception

Posted on November 20, 2011 at 11:09Hi Forum! First time I'm trying to do something with interrupts, and I get a HardFault Exception :) I'm using the IAR Workbench 6.3 with the STM32DISOVERY_VL - EvalBoard. Here's the main-function code (completely ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.