STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USART BAUDRATE-Problem

Posted on November 19, 2011 at 16:18Hi Everbody!I'm trying to set up an USART Connection to my Notebook. Everything works fine but does anyone have a clue why I have to multiply the baudrate-setting with 3 to get the correct baudrate? for Example:  ...

flash86 by Associate
  • 1915 Views
  • 3 replies
  • 1 kudos

GPIOs not functioning, what gives ?

Posted on November 19, 2011 at 15:02All, I`m fairly new to the STM32 family, not new to C or other micros: I use: Keil Lite: V4.22.22.0, 4.22a with an ST-Link, this all works and compiles etc. I can run code on my board no problem !! Now I`m trying ...

benbb by Associate II
  • 1495 Views
  • 3 replies
  • 0 kudos

EBV STM32 Design Contest - Win a Harley Davidson !

Posted on October 29, 2010 at 13:33This Could Be Your Harley Davidson!  EBV Elektronik and STMicroelectronics make it happen! Release your creativity with STMicroelectronics’ STM32 microcontrollers. Convince our panel of judges that your STM32F-base...

0690X00000603BnQAI.jpg

SDIO command CRC error on ACMD41

Posted on November 07, 2011 at 22:59When single stepping through the initialization commands for the SDIO card socket (STM3210E) I notice that ACMD41 always returns a command CRC error flag.  The ST example code specifically ignores the CCRC FAIL fl...

when is SPI clock sent?

Posted on November 17, 2011 at 12:20Unfortunately I do not own an oscillope nor a logic analyzer to see this.I'm having some problem using the SPI controller to communicate with a sensor.I've managed to get some data, but not in a consistent way.In ...

salvatore by Associate II
  • 1756 Views
  • 2 replies
  • 0 kudos

FSMC problem with low address

Posted on November 17, 2011 at 15:38When try to access to SRAM through FSMC (SRAM example from IAR 6.1) I don't see any address on  ADDRESS 7:0. Only high frequancy (> 10 MHz) peaks and splashes. With ADDRESSes 20:8 all OK. With DATA BUS all OK.  Re...

milds by Associate II
  • 1345 Views
  • 2 replies
  • 0 kudos

STM32F4 Discovery AWD IRQ

Posted on November 15, 2011 at 14:41I have been able to successfully setup the ADC3 to set the SR, AWD flag when an input exceeds my threshold set.  What I am now looking to do is put the processor in sleep mode (via __WFI();) and then have it wake ...

How to unbrick?

Posted on November 15, 2011 at 00:41I previously posted[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/5V pin no longer supplies 5V; other problems too&FolderCTI...

mastyskal by Associate II
  • 2156 Views
  • 3 replies
  • 0 kudos

STM32F103ZE ARM FLY

Posted on November 17, 2011 at 12:06Excuse. What means PC 1 ADC123_IN10 in the table of gpio of stm32f103ze (arm fly).Means that the pin PC1 is the Pin of the ADC channel 10?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.