2011-11-21 5:27 AM
I test the USB HOST HID example with STM32F207,a keyboard is connected to USB FS port.
When the program is executed, the keyboard can be recognized by STM32F207,and LCD display message:HID device:keybd,but it doesn't work.Hit any key on key board, MCU reset.The example is downloaded from ST:STM32_F105-07_F2xx_USB-Host-Device_Lib_V2.0.0
Is there anybody have encountered this problem?
ADD?Erik,I'm sorry for the ad and I have deleted it from here.Just technology.
#stm32f207
2011-11-21 11:20 PM
Yes, it's from Embest, a Chinese company. This platform is low-cost and good for evaluate STM32F207xx series processors.
2011-11-22 6:12 AM
I would doubt the honesty of a company that see fit to hijack a user forum for an ad.
ErikWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.