STM32F2XX Ethernet IAP
Posted on December 06, 2011 at 15:31I've tested the F2xx IAP over ethernet and it didn't work for me, the communications works okay, but the flash erase routine doesn't work. Has someone tested this application?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on December 06, 2011 at 15:31I've tested the F2xx IAP over ethernet and it didn't work for me, the communications works okay, but the flash erase routine doesn't work. Has someone tested this application?
Posted on November 17, 2010 at 08:08AN2799 - STM32 and STPM01 - Source Code? #unavailable-resources
Posted on December 07, 2011 at 00:25Hi, i want to know how to setup my stm32f103ze (HD) project correctly to 16mhz HSE. I build up a device with 16mhz NOT 8mhz. I want to use USB and USART too. It would be nice to have a helping hand. with regards s...
Posted on December 07, 2011 at 00:18On an STM32F103Z (ST3210E eval) I set up TIM4 in encoder mode, QEI interface with phase A on CH1 and phase B on CH2. Encoder mode is T1T2, triggering on falling edge of either phase. The encoder is a 400 positio...
Posted on December 06, 2011 at 00:55Hi, I'm trying to implement a sensor network. I know that I must use DMA to be able to work with multiple ADC channels. Since this is a school assignment, I'm not allowed to use any libraries. For some reason I'm ...
Posted on October 26, 2011 at 16:11Hi again guys, I have previously had some issues with the SDIO that have been fixed. Recently I moved my SDIO test application into my large application and have been having a strange issue writing to the power reg...
Posted on December 01, 2011 at 06:29First of all sorry for English and messy explanation. One of EXTI channels configured as interrupt on falling edge. EXTI ISR toggles GPIO(set/reset) pin and resets EXTI pending bit. I measured time between these ...
Posted on December 01, 2011 at 14:32OK so I got the USB library with custom HID example (from ST) and uCOSII in IAR v6 compiling/linking/downloading, however the USB does not enumerate properly. I assume that I have got the setup/architecture wrong...
Posted on November 25, 2011 at 13:16Hi. This is the first time I write in this forum. I must read 6 analog signals, 3 from an acelerometer and 3 from a gyroscope, every 20 ms. I am using PC1-PC3 and PA1-PA3 (STM32 Discovery VL), so this is my config...
Posted on November 23, 2011 at 02:17Hi All, On one of my projects I'm using external watch crystal (32768Hz) as LSE clock to the RTC and all works well. What I now need to do is have the RTC continue to work when the external watch crystal fails. My...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.