2011-12-06 6:31 AM
I've tested the F2xx IAP over ethernet and it didn't work for me, the communications works okay, but the flash erase routine doesn't work.
Has someone tested this application?2011-12-06 10:56 PM
- check the STM32 EVAL jumpers setting
- which FW version you are using - which protocol do you use http or tftp2011-12-07 4:33 AM
I'm using a custom board. I tried with both protocols. I noted that the erase flash function is called but it doesn't erase the flash.
This application worked for you?
2011-12-07 4:55 AM
I am using ST EVAL, it works well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.