STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Possible to avoid FLASH_Erase() stall on stm32f103?

Posted on December 08, 2011 at 20:04Hi, I'm using ADC with DMA and periodically erasing the flash pages. But the dma interrupt is not fired while i'm erasing the flash pages. I'm also using a lot of flash constants in my code. Is it possible to avo...

tedmosby by Associate
  • 1404 Views
  • 3 replies
  • 0 kudos

Listening SPI communication between two ICs

Posted on December 08, 2011 at 22:01hi everyone,Two boards communicate via SPI, I try to read what master sends to slave and what slave responds with my STM32 eval board.I simply connected 3 wires to CLK, CS and MOSI lines of master IC to three GPIO...

STM32F1/F4 incompatible I/O

Posted on December 08, 2011 at 19:32From their respective RMs: STM32F1... 0x4002 2000 - 0x4002 23FF Flash memory interface STM32F4... 0x4002 2000 - 0x4002 23FF GPIOI Thus a project predicated on STM32x compatibility must have at least different I/O ...

picguy2 by Associate II
  • 909 Views
  • 2 replies
  • 0 kudos

STM32f4 discovery timing problem

Posted on December 06, 2011 at 10:43I tried to build examples from stm32f4discovery_fw package for stm32f4-dicovery board. And I have a incorrect CPU timing settings. Some examples. I tried to make TIM_PWM_Output example with 2.5kHz PWM.   /* Comput...

glory_man by Associate II
  • 1276 Views
  • 3 replies
  • 0 kudos

how to debug (terminal) a UART modul connected to usart2 ?

Posted on December 07, 2011 at 02:00Hi, its me again :) i have my stm32f103ze USART2 with 38400 baud connected to a bluetooth modul that uses rx, tx, rts, cts. I must send some commands to the bluetooth device via USART:    /* USART2 Clock an*/     ...

sam239955 by Associate II
  • 1537 Views
  • 3 replies
  • 0 kudos

3.5'' & 4.3'' TFT LCD with Touch & MCU Interface!

Posted on December 06, 2011 at 15:283.5'', 4.3'' and 7'' TFT LCD modules with Touch Panel & LCD Controller (such as K350QVG-V1-F / K350QVG-V2-F) are provided. They have true TFT LCD colors and 8-bit/16-bit 8080 system or 3-wire/4-wire SPI interface ...

sales23 by Associate II
  • 1325 Views
  • 1 replies
  • 0 kudos

Looking for CAD Symbols

Posted on December 07, 2011 at 19:58I'm trying to locate CAD Symbols for the SMT32 family. I'm currently using Eagle/Cadsoft, with Microchip I download a file then use Ultra Librarian to convert to Eagle.   #cad-symbols-pad-layout

KevinA by Senior
  • 682 Views
  • 0 replies
  • 0 kudos

Stm32F2 : Ethernet start up infinite Loop

Posted on September 30, 2011 at 20:33Hi I have a problem in Ethernet start up using LWIP. the program always stick in a infinite loop in below line :while (ETH_GetSoftwareResetStatus () == SET) what is problem and what is this line means ? i use an...

DAC Example code

Posted on December 07, 2011 at 13:00HiDoes anyone know where I can find example code of using the DAC? I only found application AN3126 pdf but there was no firmware to go along with it.Any help would be appreciated. I've checked out the STM32 librar...

apatel by Associate II
  • 1399 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.