STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Am I right initialize I2C and read bytes?

Posted on December 06, 2011 at 18:19Hello. I have a device connected to stm32 through I2C1. Am I right initialize it?&sharpdefine DEV_ADDR 0x53uint8_t I2C_ByteRead(uint8_t Addr){ uint8_t tmp;    while(I2C_GetFlagStatus(I2CG, I2C_FLAG_BUSY)); // Whil...

Missing data on the SPI bus?

Posted on December 09, 2011 at 20:57 I have a Max3107 UART hooked up via the SPI1 bus on a STM32F103ZG. Currently, I can configure the UART, write data out and receive it. I'm trying to implement trigger interrupts because the UART has a 128 word...

thebooney by Associate II
  • 2333 Views
  • 5 replies
  • 0 kudos

STM32F107 IWDG does not make a reset

Posted on December 12, 2011 at 16:08Hello, I'm using the ST libraries to initialize the IWDG  with following code:  IWDG_WriteAccessCmd(IWDG_WriteAccess_Enable);   IWDG_SetPrescaler(IWDG_Prescaler_128);   IWDG_SetReload(0x400);   IWDG_ReloadCounter(...

hhosburg by Associate II
  • 1120 Views
  • 2 replies
  • 0 kudos

to connect to CN5 I need Micro-A plug not Micro-B

Posted on November 30, 2011 at 21:04In the User manual UM1467 (Getting started with software and firmware environments for the STM32F4DISCOVERY Kit) on page 4 under 2.1 ''System requirements'' it says:  'USB type A to Micro-B' cable, used to connect...

TIM4 Missing Update Interrupt

Posted on December 06, 2011 at 10:12The follow ISR capture an event incoming on TIM4_CCP2, and each 8 of this events the register oldCCP is subtracted from CCR2, this value is strored in loop_buf[cyc][lb_index], the value of CCR2 updates oldCCP, and...

STm32F407 LQFP176 has just 144pin in Datasheet????

Posted on December 10, 2011 at 06:26Hi, I want to make a library for EAGLE of the STM32F407IGT6 (LQFP176). On Site 142 of 154 in the datasheet, the lqfp176 package has just 144pins, is that correct or a mistake by ST? with regards alex  

sam239955 by Associate II
  • 1827 Views
  • 4 replies
  • 0 kudos

how to capture signal at rate 3 mbit/s

Posted on December 09, 2011 at 23:23hi,i have a signal to rate at 3mbit/s. The clock and signal are separate on two line.i tried to use connect EXTI on the clock. When i have a interrupt, i read the PIN where the signal's. This solution don't work.S...

max flow with lwip, for 4 tcp serveur

Posted on November 18, 2011 at 14:36hi,sorry for my english, but i'm french.I use the stack LWIP with stm32F107VC. I have create 4 TCP serveur (port 5001,5002,5003,5004).When a connect client of port TCP (exemple 5001), i send a string (1400 bytes) ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.