2010-05-23 2:18 PM
Stop mode problem
2011-05-17 4:52 AM
I forgot to mention that I currently setup the clock to the internet time via the network at every hour. Could it by setting the RTC clock using RTC_SetCounter() without the RTC_WaitForLastTask() be a problem and causing this intermittent problem?
2011-05-17 4:52 AM
There is a problem with how you are wrapping the RTC_Counter(), certainly one that might cause a stop time exceeding 24 hours. Another that would cause the wrap to fail if the counter ever exceed the rollover value.
Also if you are setting the time, from say NTP, why wouldn't you use the whole 32-bits of the RTC and track the time/date2011-05-17 4:52 AM
Hello,
for everyone who has this problem with RTC_SetCounter .
I found mistake in Examples from STD_Periph_Lib.
If you want change RTC_SetCounter you have to write your code like this:
if (RTC_GetCounter() == 86399) //Decimal value of 23:59:59 ((23*60 + 59)*60 + 59)
{
PWR_BackupAccessCmd(ENABLE);
/* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();
/* Set initial value */
RTC_SetCounter(0x0);
/* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();
PWR_BackupAccessCmd(DISABLE);
}
It works for me.
2011-05-17 4:52 AM
if (RTC_GetCounter() == 86399) //Decimal value of 23:59:59 ((23*60 + 59)*60 + 59)
{
PWR_BackupAccessCmd(ENABLE);
/* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();
/* Set initial value */
RTC_SetCounter(0x0);
/* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();
PWR_BackupAccessCmd(DISABLE);
}
And what exactly happens with sloppy code like this when the CPU happens be asleep over the Midnight event? Or asleep for a couple of days/weeks? Seem also to remember that 00:00:00 is equivalent to 24:00:00 not 23:59:59, or perhaps you have some leap second event you are handling.2011-05-17 4:52 AM
And what exactly happens with sloppy code like this when the CPU happens be asleep over the Midnight event? Or asleep for a couple of days/weeks?
Seem also to remember that 00:00:00 is equivalent to 24:00:00 not 23:59:59, or perhaps you have some leap second event you are handling.
I'm sorry,
I thought that he has problem with RTC_SetCounter. For first time when I tried write code for RTC Interrupt, I used example from Std_Periph_Lib. It not worked for me.
The RTC reset counter part of his code look like ST's example.
And yes, you're right. This solution is very bad. It's better to calculate date and time from seconds without resetting rtc counter.
2011-05-17 4:52 AM
2011-05-17 4:52 AM
It's a 32-bit counter, it does not stop at arbitrary values, when it gets to 0xFFFFFFFF it then wraps to 0x00000000. If the RTC prescaler is in seconds, this occurs in just over 136 years.
Thus my point about sloppy code, and missing the increment across the 24 hour threshold, should you only be interested in Time-Of-Day. If you do an equality check, and you miss the exact second you are checking, it will be 136 years before the check will match again. If you want to confine it to 24 hours, you should always check >= 86400, in which case you should then subtract 86400 from the RTC. If it was out for several days, you might have to repeat the check/subtraction until the number is in scope. You can enumerate the days. Generally it would be better just to use the 32-bit value to record the time and date, from some epoch date, like the one used by UNIX, or based from 2000 or 2010. You would then be able to do simple math on the RTC counter and figure how many seconds (hours, days, weeks, or get a tad more complicated for years, decades, centuries) had elapsed while asleep. The leap year math also gets significantly simpler if your supported epoch is from 1-Jan-2000 to 31-Dec-2099. (hint every 4 years, but 2100 is NOT a leap year)2011-05-17 4:52 AM
2011-05-17 4:52 AM
The STM32's RTC is not a calendering device. It does not track days, weeks, or other earth/human representations. It counts seconds, or other units, depending on the oscillator and prescaler.
The caution is specifically for those who want to imagine the RTC as a Time-Of-Day counter. This model will break for them, if the part ticks past the 24-hour threshold overnight, or is left asleep for long periods. Such overflows must be specifically handled manually, by pulling the value into scope. If left unchecked, an alarm will NOT fire everyday, but once every 136 years. Personally, I find this model to be particularly stupid, and prone to breakage or poor implementation. Time is linear, and with a 32-bit counter you can model a 136 year period, and determine with little effort the date, day of week, month of year, and year. You can certainly make the STM32 report time and date exactly like you can on a PC. If you set the RTC correctly, or periodically sync it with an external source, you'll be fine.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.