STM32F4 Discovery
Posted on May 12, 2012 at 08:50hii am starting with STM32F4 Discovery i need to know which development software is the bestkeil or the attolic, thank you
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on May 12, 2012 at 08:50hii am starting with STM32F4 Discovery i need to know which development software is the bestkeil or the attolic, thank you
Posted on May 20, 2012 at 07:45Hi I recently recieved an STM32F0 discovery board and got to doing some testing on it with the gcc toolchain found at:https://launchpad.net/gcc-arm-embedded/4.6/2011-q4-major I discovered that the ''startup_stm32f0xx...
Posted on October 22, 2011 at 02:19HiI have eclipse 3.6 with GNU ARM C/C++ development support configured.However, it can generate hex file with warning: cannot find entry symbol Reset_Handler; defaulting to 08000000. Not sure will this effect the h...
Posted on May 17, 2012 at 02:36Does anyone know how to produce a solid 3-phase implementation via the timers on these STM32F4-Discovery? I'm wanting to be able to produce a simple 3-phase digital signal upon 3 output channels are varying frequencies...
Posted on May 18, 2012 at 14:37Hi everyone,I m trying to be in USB Mass storage Mode by default, and being able to do DFU action upload and download.I read that I have to disable all other interface to get in DFU mode.Thus, I wanted to use DFUSE to ...
Posted on May 18, 2012 at 21:45 Hello -- We're trying to bring up FreeRTOS on our STM32F103c8 micro. In the function vPortStartFirstTask (file portasm.s) there is an SVC call as follows: cpsie i 0x8002efe: 0xb662 CPSIE i svc 0 0...
Posted on May 16, 2012 at 23:26Hello I have a problem with calculating internal temperature with STM32. When processor VCC is 3.3V everything is ok - temperature is almoast accurate with wide temerature range. But whet processor VCC is below 3V temp...
Posted on May 16, 2012 at 06:43Dear all, I'm using `Keil uVision` with gcc toolchain (Sourcery Codebench lite for ARM EABI) to program the `STM32F4 cortex M4` chip. The compiler control strings I have set are: -march=armv7e-m -mfpu=fpv4-sp-d16 ...
Posted on May 17, 2012 at 03:39What's the difference between EXTI_Mode_Interrupt and EXTI_Mode_Event? #external-interrupt
Posted on May 16, 2012 at 15:12Hello, The Cortex M3 have the �ID Unique device ID register (96 bits) �, this number give to the user application technical information about the Cortex M3 mounted in the PCB ?. Extract from the datasheet RM008 revisi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.