2012-05-16 5:36 PM
Does anyone know how to produce a solid 3-phase implementation via the timers on these STM32F4-Discovery? I'm wanting to be able to produce a simple 3-phase digital signal upon 3 output channels are varying frequencies from low Hz to nothing more than 1 MHz. So, nothing crazy, but the part I'm wondering about mainly is how to 'best' produce the 3-phased signals upon the 3 output channels. Any ideas guys?!?
Thanks in advance!!! #3-phase-timer-stm32f4discovery2012-05-16 5:50 PM
I believe DM00037051.pdf would cover what you want.
page 29 do a google I apologize, I have not ported my 56F103 code over yet.2012-05-16 6:27 PM
Ok, I was thinking that, for instance, TIM1, all its channels had to be at the same time base, but apparently not, its 4 channels can have different prescalers. Still much to consider, but thanks for the guidance!
2012-05-18 7:19 PM
Ok,
I got it all working now, the 3 phase generation, it was a bit easier than I had thought, amazing what a few days can do lol! Not only that, but I can change the frequency of the 3 phase signal on the fly via a usb connection to my pc, and also have a nice lcd where the current frequency is displayed. All controlled by this awesome STM32F4-Discovery!!! Thanks guys!2012-05-18 8:08 PM
If anyone is interested in generating 3 phase digital signals, you merely have to make sure that you use compare values that are divisible by 3 exactly, to ensure perfect 3 phase generation, in addition, pattern your ARR accordingly...
Here are some key snippets below... snippet from timer.c: ---------------------------------------------------------------------------------------------- TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; __IO uint16_t CCR1_Val = 65534; __IO uint16_t CCR2_Val = 43689; __IO uint16_t CCR3_Val = 21844; uint16_t PrescalerValue = 0; /* Private function prototypes -----------------------------------------------*/ void Setup3PhaseTimer(void); void NVICConfig(void); /* Private functions ---------------------------------------------------------*/ void Setup3PhaseTimer(void) { NVICConfig(); /* Turn on LED4, LED3, LED5 and LED6 */ STM32F4_Discovery_LEDOn(LED4); STM32F4_Discovery_LEDOn(LED3); STM32F4_Discovery_LEDOn(LED5); PrescalerValue = (uint16_t) ((SystemCoreClock / 2) / 250000) - 1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 65534; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* Prescaler configuration */ TIM_PrescalerConfig(TIM3, PrescalerValue, TIM_PSCReloadMode_Immediate); /* Output Compare Timing Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM3, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Disable); /* Output Compare Timing Mode configuration: Channel2 */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR2_Val; TIM_OC2Init(TIM3, &TIM_OCInitStructure); TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Disable); /* Output Compare Timing Mode configuration: Channel3 */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR3_Val; TIM_OC3Init(TIM3, &TIM_OCInitStructure); TIM_OC3PreloadConfig(TIM3, TIM_OCPreload_Disable); /* TIM Interrupts enable */ TIM_ITConfig(TIM3, TIM_IT_CC1 | TIM_IT_CC2 | TIM_IT_CC3, ENABLE); /* TIM3 enable counter */ TIM_Cmd(TIM3, ENABLE); } void NVICConfig(void) { NVIC_InitTypeDef NVIC_InitStructure; /* TIM3 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); /* Enable the TIM3 gloabal Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); } -------------------------------------------------------------------------------------------- snippet from stm32f4xx_it.c: -------------------------------------------------------------------------------------------- void TIM3_IRQHandler(void) { if (TIM_GetITStatus(TIM3, TIM_IT_CC1) != RESET) { TIM_ClearITPendingBit(TIM3, TIM_IT_CC1); STM32F4_Discovery_LEDToggle(LED4); } else if (TIM_GetITStatus(TIM3, TIM_IT_CC2) != RESET) { TIM_ClearITPendingBit(TIM3, TIM_IT_CC2); STM32F4_Discovery_LEDToggle(LED3); } else if (TIM_GetITStatus(TIM3, TIM_IT_CC3) != RESET) { TIM_ClearITPendingBit(TIM3, TIM_IT_CC3); STM32F4_Discovery_LEDToggle(LED5); } } ---------------------------------------------------------------------------------------------We’re moving the ST Community to a new platform to give you a better and more reliable community experience.