STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Difficuly of implementing nand driver on STM32F205ZG

Posted on May 15, 2012 at 08:47Hi all, Now, I'm trying to implement nand driver of  SAMSUNG K9K8G08U0D (SLC, 1GBYTE) on STM32F205ZG cpu. However, it not easy to do it. First, reading device ID is OK. Second, block erase function is also OK. But,...

kpkang by Associate
  • 2206 Views
  • 2 replies
  • 0 kudos

Need for Backup registers > 4KBytes

Posted on May 15, 2012 at 19:31I wonder if someone could help me. I need to save, to retain ''some'' variables of my applications, but the 4Kbytes from the Backup registers is too few for what I need. So I would like to ask if there is another way t...

tecnico23 by Associate II
  • 2335 Views
  • 12 replies
  • 0 kudos

Slope of internal temperature sensor

Posted on April 10, 2012 at 11:25Hello, we are using the microcontroller STM32F100C6T7 in our design. While trying to do something with the internal temperature sensor we noticed that the slope we measured doesn't correspond with the specified slope...

kbroger by Associate
  • 2224 Views
  • 4 replies
  • 0 kudos

not getting DMA interrupts for some reason

Posted on May 15, 2012 at 17:13i've faced a couple of problems, trying to launch a MT9D111 camera along with STM32F217ZG microcontroller through DCMI interface. I've got all the interrupts from DCMI, but i can't catch any interrupt from DMA, althoug...

Determining the value of VECT_TAB_OFFSET

Posted on May 15, 2012 at 02:39I recently had a problem where my SysTick_Handler wasn't firing.  The solution was to change the VECT_TAB_OFFSET from 0x00 to 0x4000.  How does one determine what his value should be?  If it can be different based on o...

mfranklin by Associate III
  • 1170 Views
  • 1 replies
  • 0 kudos

Problem of 3-Wire Fan Speed Measurement & Control

Posted on May 13, 2012 at 12:58Recently I was designing a subsystem of closed loop fan control.  This diagram shows the method: using a channel of PWM to control the speed (GND method), and a channel of capture module to measure fan speed. The box o...

0690X00000602l3QAA.jpg 0690X00000602kyQAA.jpg

Failure loading STLinkUSBDriver.dll

Posted on May 13, 2012 at 22:33did a google search none of the links worked. I installed st-link_v2_usbdriver.zip, ST-LINK_Utility_V2.2Patchv10.zip I searched my computer for STLinkUSBDriver.dll and could not find it. I was able to install the STLin...

bjfree by Associate II
  • 5433 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.