STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Usage of SPI1 and SPI2 on STM32L-Discovery

Posted on May 30, 2012 at 18:19Hi,I am trying to understand the operation of the STM32L-Discovery with the aim of setting up SPI transactions between two STM32L-Discovery devices.When I look at the specs:1) SPI1:SPI1 is defined on PA4, PA5, PA6 and ...

gavin2 by Associate II
  • 3902 Views
  • 4 replies
  • 0 kudos

Nichelite / IAR EW / IAR KickStart Kit for STM32F107VC

Posted on May 08, 2012 at 23:24Hi All, I'm trying to get Nichelite working with the IAR KickStart Kit for STM32F107VC but so far I'm failing and could do with some help. Has anybody managed to get this going? So far, I've got everything to compile b...

stforum23 by Associate II
  • 1614 Views
  • 2 replies
  • 0 kudos

SPI Flash

Posted on May 31, 2012 at 10:04Hello I am working on LCD project (Fractals) and i need large buffer for storing iteration values, so i can calculate fractal and when paint it. I need to store 8b number, total of 130560. so what would be around 1Mb. ...

linas2 by Associate II
  • 2057 Views
  • 3 replies
  • 0 kudos

Reading from SPI (Bidirectional one line)

Posted on June 02, 2012 at 05:01 Hi all, I'm trying to use the SPI interface of a TFT controller that uses only one line for write and read. I have the following problem: 1)First I set the SPI direction as Tx and write one byte data to...

0690X00000605UAQAY.png
talhakoc by Associate
  • 1411 Views
  • 1 replies
  • 0 kudos

ADC Calibration

Posted on May 23, 2012 at 16:31 I am trying to figure out if the ADC calibration is reset when the ''ADC_DeInit'' function (from the peripheral library) is called after previously calibrating. My guess is that it does, since the ADC_DeInit funct...

tbenson by Associate II
  • 3563 Views
  • 5 replies
  • 0 kudos

Wake up from STOP MODE STM32L152

Posted on May 31, 2012 at 10:05Hi all, I have to be sure before I will make another step in my project: Can I wake up the STM32L152 from the STOP mode by any edge on any pin? In other words: can I configure any pin as input to wake up from STOP mode...

olek by Associate
  • 1525 Views
  • 2 replies
  • 0 kudos

Simulation Problem in keil 4.2V

Posted on October 15, 2011 at 10:03I could not simulate my code written for STM32F205ZE using keil 4.2V.Following is error code it is showing, when I start debug session.*** error 65: access violation at 0x0000000C : no 'read' permissionIf I try to ...

k_hraj by Associate II
  • 1748 Views
  • 3 replies
  • 0 kudos

STM32 power-on problem

Posted on May 30, 2012 at 10:45I have designed a PCB that has an http://www.st.com/internet/mcu/product/250189.jsp microcontroller. It kind of works, but the micro has a weird power-on/startup problem. Basically, when the power is applied the micro ...

field gpio_type could not be resolved error

Posted on May 28, 2012 at 18:51Why should the App.h file with :   /// PORTA[0..15] = Available :   RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOA , ENABLE);    GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin...

jlchoobs by Associate II
  • 1174 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.