STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

issue of reading RTC

Posted on June 06, 2012 at 08:48Hi All,I am wondering if there is an internal interlock that prevents the RTC from being updated while the registers (RTC->CNTH and RTC->CNTL) are being read.There is a situation where RTC->CNTH has been read RTC then...

markaren1 by Associate II
  • 1128 Views
  • 1 replies
  • 0 kudos

Starting with a STM32F100CBT6B

Posted on June 05, 2012 at 21:30Hello, I am new to ST micros and this is my first attempt to design a board based on a 32-bit microcontroller. I've designed a very simplistic circuit with all of the GPIO ready for use for experimenting with breadboa...

gmwralhs9 by Associate II
  • 2488 Views
  • 4 replies
  • 0 kudos

gdb backtrace/ exception handlers

Posted on May 24, 2012 at 20:20Very occasionally, my code takes an unexpected exception and ends up in a default handler :)I'd like to write such a handler so that GDB can successfully unwind the stack.  For example,default_handler (void) { asm(''ld...

USART3 interrupts - stm32f4xx

Posted on June 04, 2012 at 05:32Anyone have any example code for USART Interrupts? I've tried finding some example code to work off of. 

spyguy99 by Associate II
  • 2931 Views
  • 7 replies
  • 0 kudos

linux toolchain for smt32f4

Posted on June 04, 2012 at 10:55Hi, i'm new in the arm world, and i have bought a smt32f4 (maybe not so good for a kickstart, but i'll survive). i'm compiling the gcc arm eabi toolchain, but i've also seen the Yargarto, is quite used here. For my fi...

bifrost by Associate II
  • 1366 Views
  • 3 replies
  • 0 kudos

SDIO+eMMC

Posted on June 05, 2012 at 09:10Hi Andrew, I work on an application with a STM32F207 and a eMMC memory (THGBM4G8D4GBAIE). I have some questions for you. Do you use a file system ? which ? I use the RL-Flash from Keil but it seems to not support sect...

STM32F105 Spontaneously Erased

Posted on June 02, 2012 at 01:27I have not received back two units with an STM32F105 that appears to have been erased in the field.  The units are sealed, and show now signs of tampering.  When received there is no response.  When we connect the JTA...

Stephen28 by Associate III
  • 1522 Views
  • 3 replies
  • 0 kudos

STM32, 'simple' issue of changing IRQ priorities (!)

Posted on June 02, 2012 at 18:46Hi All,Is there an easy way to change the priority of TMR1interrupt ? I need to change it so that it has lower priority than USART1, 2 & 3.The M3 TRM, while being quite comprehensive appears (to my simple mind) almost...

markaren1 by Associate II
  • 2564 Views
  • 4 replies
  • 0 kudos

F207 USART TXE issues

Posted on June 04, 2012 at 16:29Hello. I am seeing issues witht he TXE interrupt firing for no reason. Here is my IRQ handler: #define COM3       USART3void USART3_IRQHandler(void) {     uint8_t x;    // Get Byte from DR in case of Overrun     if (...

stbbrad3 by Associate II
  • 1761 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.