STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I NEED HELP

Posted on June 01, 2012 at 17:15Hello, I need help on my project, release is in 45 days and I still have a few bugs I can't get rid of. I'd need someone good in both soft and hardware to support me. Job is paid, of course. Thomas.

root by Associate II
  • 1120 Views
  • 3 replies
  • 0 kudos

SDIO for STM32F4 discovery

Posted on June 09, 2012 at 19:13friends i need mdk-arm project for accessing uSD card i.e SDIO for STM32F4 discovery.....its very urgent...plz someone suggest me..TIA #urgent

rishi by Associate II
  • 1277 Views
  • 3 replies
  • 0 kudos

STM32 DISCOVERY BOARD WITH STM32F10x_StdPeriph_Lib_V3.5.0

Posted on May 19, 2012 at 15:38I am new to STM32 discovery and using the program  package  STM32F10x_StdPeriph_Lib_V3.5.0. I am trying to run adc module with this package .But when, I run that code provided into example into STM32 discovery board. I...

jai23 by Associate II
  • 1679 Views
  • 4 replies
  • 0 kudos

STM32F0 Feedback

Posted on June 09, 2012 at 04:41Hi all, Is it worth considering STM32F051C for a new project? It seems to fit perfectly in our requirements but I did not find any errata sheet on the website so I am not able to confirm that it is free from any bugs ...

Is Code Sourcery worth the effort ?

Posted on May 28, 2012 at 18:28I have been using the Atollic (Lite) for my development. My Atollic Projects work great (doing USB & MMC work). But I have run out of space with the 32K limit. So I moved over recently to the Code Sourcery - or tried. ...

jlchoobs by Associate II
  • 3988 Views
  • 14 replies
  • 0 kudos

SPI reception, data shifted by one bit

Posted on June 08, 2012 at 17:42Hi,I am having some difficulty receiving SPI data correctly and I am hoping someone could help.I currently have two STM32L-Discovery boards connected via SPI with one acting as master and one as slave. My SPI transmis...

gavin2 by Associate II
  • 898 Views
  • 0 replies
  • 0 kudos

STM32 USB Host Device Library v2.1.0 with F4 support

Posted on April 03, 2012 at 19:57Hi all,I don't see this mentioned anywhere on the forum, but a new version of the STM32 USB library was released recently and it adds the long-awaited support for the STM32F4 family. I've tried it with the STM32F4-Di...

tony2399 by Associate II
  • 3748 Views
  • 8 replies
  • 0 kudos

Synchronized (Chained/Cascaded) Timers

Posted on June 06, 2012 at 18:13Newbie here...I'd like to use one timer as a prescaler for another. Both these timers (combined) will act like a single 48-bit ''uptime'' value, used for timestamping events. The master timer will be driven off APBx.I...

sacleary by Associate II
  • 1481 Views
  • 2 replies
  • 0 kudos

How to store user data in flash memory(stm32f207ig)

Posted on June 05, 2012 at 16:28Hello All,I have been trying to write into the flash(certain user data), but when i debug it i see the values being written elsewhere in other locations and sometimes in the location i have specified.The function i ha...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.