STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Evaluation Board Suggestions.

Posted on July 18, 2012 at 16:55I like the STM32F4 Discovery  for deveopment before hardware arrives.  It brings out many of the processor pins, and most of those pins are not ''hard wired'' to a function on the board.  This accomadates developing f...

I2C Slave Cannot Clear STOPF Flag

Posted on July 19, 2012 at 17:50 Hi, Another small littleconundrumI am hoping someone out there might help me solve. I have got an i2c master and slave talking to each other, I'm fairly sure the Master code is good as it's been wor...

dclark9 by Associate II
  • 1560 Views
  • 1 replies
  • 0 kudos

USB host on stm32f107

Posted on July 02, 2012 at 10:03Hello everyone! I want to create a new topic for incremental learning with usb for beginners. I've started to learn usb library, seen examples, but I have many questions. First of all, I can't undestand, how to conf...

trouble with make file.

Posted on July 18, 2012 at 22:14  The original post was too long to process during our migration. Please click on the attachment to read the original post.

arnold by Associate II
  • 2286 Views
  • 3 replies
  • 0 kudos

Parallel Interface on the STM32F4

Posted on July 18, 2012 at 19:47Hello,I'm wondering how to create a parallel interface on the STM32F4Discovery Board, if possible. As far as the application, I would like to connect the Discovery to an external ADC evaluation module from TI (ADS855x...

xtaega by Associate
  • 2842 Views
  • 2 replies
  • 0 kudos

Asynchronous SCLK when using SPI

Posted on July 18, 2012 at 13:41I am having some problems in that the SCLK signal for my SPI (when using either SP1 or SPI2) appears to be incorrect. Although the period is stable throughout and as I would expect, the clock pulse itself is non symme...

gavin2 by Associate II
  • 1367 Views
  • 2 replies
  • 0 kudos

Problem receiving data on USART1

Posted on July 18, 2012 at 12:37 Hello, I am using the STM32L-Discovery board and try to transmit / receive data via USART1. My problem is that the controller does nor react on data sent from the PC, but if I send one byte from the contr...

USB FS setup packets and buffer overrun

Posted on July 16, 2012 at 07:23Hi all! I have two questions on how to interpret the documentation for the USB FS device macrocell in medium density devices. 1. The section on OUT transactions states that when a buffer is overrun (i.e. the data payl...

ashibakov by Associate II
  • 1801 Views
  • 2 replies
  • 0 kudos

STM32F4Discovery Virtual COM port

Posted on July 10, 2012 at 22:00Hello! I would like to send simple data from STM32F4Discovery to PC (''Hello World!'' every second would be perfect for beginning). I am pretty lost here. How do I create virtual COM port? When I connect PC to the bo...

jurij by Associate II
  • 5040 Views
  • 18 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.