2012-07-18 7:55 AM
I like the STM32F4 Discovery for deveopment before hardware arrives. It brings out many of the processor pins, and most of those pins are not ''hard wired'' to a function on the board. This accomadates developing firmware modules on the Discovery board that use the same peripherals / pins as the custom hardware design does.
The discovery board comes close to being ideal but falls a bit short. A small number of the pins are hardwired to on board chips. For example, I believe USART1 is hard wired to the USB OTG function. For UASART debug I removed a couple components from the board. Additinally, some of the many pins are not brought out. More specifically ports beyond E are not available at the edge headers. For the prehardware firmware development I just completed, the ideal board:I really like the STM32F4 Discovery. I am only identifying how a board might better satisfy the specific customer need of firmware development before prototype boards are available.
John2012-07-18 8:42 AM
I wired up USART2 for debug.
Different boards tickle different needs, here are a couple I've run across in my searches.http://www.wvshare.com/product/Open407Z-Package-B.htm
https://www.olimex.com/dev/stm32-h407.html
http://www.hotmcu.com/hystm32f4xxcore144-coredev-board-p-10.html?cPath=1_20
http://www.waveshare.net/shop/Core407V.htm
http://www.wayengineer.com/index.php?main_page=product_info&cPath=50_66&products_id=569
2012-07-19 1:45 PM
Although the Discovery boards don't have ''jumpers'' in the traditional sense of 0.1''-pitch pins with removable links, they do have little ''solder-bridge'' links which can be used to disconnect unwanted circuitry - see the User Manual (which includes schematics) for details...
(I don't find this a very user-friendly approach, but it is the way that things are going these days - ST are by no means alone in adopting it...)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.