2012-08-10 5:46 PM
Hello,
1. What is the maximum SPI speed I am suppose to achieve with the 8MHz HSE? 2. I would like to achieve at least 25MHz, what would it take to achieve that both code and HW? Currently with my code below I get 13MHz.void configure_spi_r(void){ //Init GPIO structure GPIO_InitTypeDef GPIO_InitStructure; //Init SPI structure SPI_InitTypeDef SPI_InitStructure; //Enable SPI clocks RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1,ENABLE); /* Enable GPIO clocks */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); //Set GPIOs GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect SPI pins to AF5 */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1); //CLK GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1); //MOSI SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Hard; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; //SPI1- for CLK, DATA, CS(DIR) SPI_Init(SPI1,&SPI_InitStructure); SPI_SSOutputCmd(SPI1,ENABLE); SPI_Cmd(SPI1,ENABLE); }2012-08-10 6:32 PM
1. SPI clock depends on APB clock. In case of SPI1 max APB1 clock is sysclock/2, so with 168MHz MCU APB1 gets 84 MHz. Max SPI clock in theory is APB/2 but due to inner MCU structure ST promised max SPI clock 37.5 MHz only.
2. So there is no problem to achieve 25Mhz. But it does not assume you'll get (37.5/8) Megabytes per second throughput. To get closer to max possible Mbps ratio use 16 bit transfer (if possible), unfold the transmission loop, use direct register access instead of functions. 3. In your initialization NSS and MISO do not used as AF pins, so it is better to leave them for a general use.2012-08-13 9:22 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.