STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 newbie question

Posted on August 24, 2012 at 09:27Hi , I'm new to STM32. Just designed a new board and assembled a prototype, but it does not work. when I connect J-link to it through SWD (three wires) interface, and start debugging, uVision4 gives these warnings: ...

cxu_dl by Associate II
  • 2807 Views
  • 4 replies
  • 0 kudos

USB Driver for STice emulator

Posted on August 22, 2012 at 19:53Look For  USB  Driver for STice emulator if there. My Windows 7 does not recognise STice Board. Please Help Tanks Abdul

gafsos by Associate II
  • 1919 Views
  • 3 replies
  • 0 kudos

stm32w

Posted on August 24, 2012 at 14:51hi i have a problem with the stm32w  mb851a i would generate a random number. i have try to use the function rand() and I include header filebut when i execute the program it jump at void __attribute__ ((weak)) Defa...

lucabe90 by Associate II
  • 1331 Views
  • 2 replies
  • 0 kudos

STM32 bootload problem

Posted on August 24, 2012 at 15:31Hi all, I have this problem: When I download my firmware on the discovery EVM (using ST-link) eve1rything goes right and when I power up again the board (after a power-off) the firwmare is present. When I do the sam...

Hard Fault on first SRAM access

Posted on August 23, 2012 at 04:51Hello,STM32L152, Rowley CrossStudio 2.3, STM32L152DEMO pcb, Using CrossConnect debugger within CrossStudio.I have seen this problem before, did not record/understand last time fixed.What will cause a hard fault on f...

STM32 Rotary Encoder config

Posted on August 22, 2012 at 18:23 I am trying to use timer 8 in Encoder mode and my setup is as follows. Pins PC8 and PC9 (timer8) are connected to a cheap 3 terminal encoder that has C pin grounded so pullups are activated on these pins. TIM...

modcan by Associate II
  • 4008 Views
  • 7 replies
  • 0 kudos

Warning: limit simultaneous DMAs to 2

Posted on January 14, 2012 at 01:53We've been working on this problem with the F2x and F4x for some time, and figure it's about time to warn others about what we've found. You can find the full details here:http://blog.frankvh.com/2012/01/13/stm32f2...

Remapping USART3 to SPI3 @STM32F107 not possible?

Posted on August 22, 2012 at 20:57Hello everyone,I am working with the STM32F107 chip on the STM32F107VC board from IAR.The evaualtion board has an LCD which has as its inputs SPI3_MOSI and SPI3_SKC. But since it needs to have 9 bit inputs, i can co...

dbeken by Associate II
  • 2202 Views
  • 6 replies
  • 0 kudos

Interfacing OV5620 sensor with stm32f103

Posted on August 10, 2012 at 13:43Hello,i have interfaced ov5620 sensor with stm32 vl discovery board.....it is a 5 MP camera sensor....the problem is i am getting multiple frames in my image...i am getting this image through video port.....can any ...

pawan by Associate
  • 1410 Views
  • 1 replies
  • 0 kudos

SPI change polarity on the fly

Posted on August 22, 2012 at 18:30Hi, I want change polarity on the fly example When I setting the SPI master, I setting ''SPI_CPOL_Low'' trasmit the 16 bit data, and work! But I need recive another 16bit data with polarity inverse ''SPI_CPOL_Hight'...

0690X00000602lmQAA.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.