2012-12-21 12:46 PM
I'm attempting to get DFU over USB working on a STM32F205VET6. Chip marking:
STM32F205 VET6 X HPABG VG KOR HP 225 Computer Windows 7 64-bit Intel Pentium dual core processor The BOOT0 input is derived from USB-VBUS, power is NOT USB. So plug in USB, power up processor. PC plays USB device connected sound, then reports ''unrecognised device''. Using a 'scope I can see several transactions on the USbus. Elsewhere I can see a reference to ''Windows has stopped this device because it has reported problems. (Code 43)''. Checking with device manager, I've tried updating the driver manually, it just reports no driver is necessary for this device. Also tried this on my laptop with windows XP, similar result although XP does report VID and PID both as 0000 (Win7 doesn't reports and VID or PID values. I can get the bootloader to work using the serial connection, so I know the BOOT0/BOOT1 pins are correct. This is on equipment provided to me for evaluation. It will need to be easily field upgradeable by users so USB is a MUST. Thanks in advance for any help/information.2012-12-21 3:21 PM
Extra info:
Serial bootloader reports: PID 0411 BID 3.3 Version 3.1 The crystal on the processor is 12.00 MHz.2012-12-21 6:01 PM
STM32F205ZCT6
16 MHz external Externally powered, not via USB BOOT0 Jumpered High Windows 7, x64, AMD Phenom II X6 VID/PID had values suitable to load the drivers, and the DFU Demo app found and programmed the device. I don't have the device in front of me right now, so can't dig into the minutia, but is was a non-painful exercise. Do you have an STM32F4-Discovery? Can you DFU program that? If that works look carefully how it's wired up, and contrast it to your design.2012-12-28 3:17 PM
I've just 'scoped the DP and DM signals. DP is OK (0 to 3 volts), but the signal on DM is -1.5volts to +1.5 volts. I've tried the obvious, different cables, different USB ports, and already tried a different PC. I've also checked for shorts on the board, nothing obvious. It looks to me as though the STM32F205 has a faulty DM pin.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.