STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 ext SRAM to SPI failure

Posted on January 26, 2013 at 20:30Hello to all, I have a design where cpu has to transfer blocks of data to a uSD card working in SPI2 mode. My routine is : static void SPIblockTxDMA(uint8_t *SD_Buffer_Tx,uint16_t Len) {   SPI_Cmd(SPI_SDMEM, DISABL...

abrous3d by Associate II
  • 1578 Views
  • 2 replies
  • 0 kudos

Data transfer between two STM32 devices using FSMC

Posted on January 26, 2013 at 22:45Hi, I'm currious if it is possible to share data between two STM32 devices, using the FSMC interface. Is it possible to configure one device as a Master and the other as a slave and use the FSMC? I would make the s...

tecnico23 by Associate II
  • 1673 Views
  • 3 replies
  • 0 kudos

STM32 Pinout tables in text or spreadsheet format

Posted on January 26, 2013 at 22:36Is there a place that one can get the pinout tables for the STM32 family devices in a format other than PDF?  The tables in the PDF datasheets and reference manuals are not easily copied to other software, and it s...

st link 20-pin jtag to 10 pin swd, can't halt the core

Posted on January 28, 2013 at 09:16Hello  everyone.I need to connect, programm and debug project on one board with 10 pin swd.1. vcc +3 V2. tms_swdio (pulled up to +3V throught 5.1 kOhm resistor)3. gnd4. tck_swclk  (pulled up to +3V throught  5.1 kO...

TIM2 Output Only CH3/4

Posted on January 11, 2013 at 11:12Here is a STM32F103-question.TIM2 is using TIM_OCMode_PWM1 and TIM_OPMode_Single (one-pulse mode).Im using TIM2 CH1 for (internal) triggering ADC injected reads using a compare. Im using TIM2 CH2 for (internal) tri...

DMA Configuration from SRAM to SD Card

Posted on May 30, 2012 at 01:55I am new in developing firmware by using STM32L152VBT6. I need to configure DMA to transfer data from SRAM to SD Card. The data would be {1, 2, 3, 4, 5, 6, 7, 8, 9, 0}. However, I could not write into SD Card and I cou...

cng by Associate II
  • 5443 Views
  • 12 replies
  • 0 kudos

FFT/IFFT transform

Posted on January 27, 2013 at 23:13Hi!I'm trying to make forward/inverse FFT. The target is to compare, that data before, and after FFT/IFFT are equal.// Vars definitionq15_t ADC_input[512];q15_t RFFT_output[1024];arm_rfft_instance_q15 S;arm_cfft_ra...

ma.x9 by Associate
  • 700 Views
  • 0 replies
  • 0 kudos

FFT/IFFT transform

Posted on January 27, 2013 at 23:03Hi!I'm trying to make forward/inverse FFT. The target is to compare, that data before, and after FFT/IFFT are equal.// Vars definitionq15_t ADC_input[512];q15_t RFFT_output[1024];arm_rfft_instance_q15 S;arm_cfft_ra...

ma.x9 by Associate
  • 958 Views
  • 0 replies
  • 0 kudos

stlink v2 error

Posted on January 24, 2013 at 16:59hiI am using STM32W108CB and made my own pcb. I've stlink v2 and want to use it as Serial Wire Debugger.When I press 'connect to the target' in stlink utility I get message 'Internal command error'.I've tried to se...

10bec062 by Associate II
  • 2133 Views
  • 4 replies
  • 0 kudos

STM324xG-eval No sound

Posted on January 27, 2013 at 15:58 Hi, I am trying to play some audio on my evaluation board,but no luck : I have a buffer that contain slices from various wav files,the buffer located in the external RAM ( if it matters) , and i tr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.