2013-01-25 8:12 AM
Hi All,
According to the apps note AN4061, a page erase should only occur when one page is full. For instance, after the first run and the memory is formatted, page0 is marked as VALID_PAGE, and page1 is marked as ERASED. However on page 7, of the apps note, it shows page1 being erased every time at power up, regardless if page 0 is full. This is exactly what the code does. Does a flash erase actually occur in this case, if page 1 contains all FF's? Otherwise surely the calculations on page 17 cannot apply if page1 is erased at power up every time? Perhaps I have mis-understood? BR's, Martin.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.