STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bootloader and code protect

Posted on February 02, 2013 at 10:43Hello ; It was not clear to me in the documents ; we are loading the program through usart3(stm32f407)  ; so can we still have the code protect fuse? I mean we dont our code to be copied; when using Jtag it is ok...

sami by Associate II
  • 1034 Views
  • 2 replies
  • 0 kudos

GPIO microcontroller STM32F047VGT6

Posted on February 03, 2013 at 10:19I use a microcontroller STM32F047VGT6 all alone without the kit board I want to use GPIO    (I want to interface the GPIO Pin )  .. Is what I connects Pin  directly without any electronic component?? #interface...

hatem by Associate II
  • 1167 Views
  • 1 replies
  • 0 kudos

Using SDIO instead of SPI in STM32

Posted on January 09, 2013 at 14:14 Hi all, How can I use the SDIO to access to an uSD card with EFSL filesystem. The example I have is using EFSL with SPI as communication interface. I should have an interface.c file where I do a...

tinymanta by Associate II
  • 5394 Views
  • 11 replies
  • 0 kudos

Efficient way to implement trigonometry functions?

Posted on February 02, 2013 at 19:28Hello,I'm working on the STM32F4, and in my application i need to use atan2 and exp a very large number of times.In my initial implementation i used the stlib for atan2 and exp. Unfortunately, in the current state...

Using ST Link on Discovery board as standalone ST Link

Posted on February 02, 2013 at 09:12I have http://www.sainsmart.com/sainsmart-stm32f103rbt6-arm-cortex-m3-mini-development-board-code-jlink-v8-adapter.html (board only), and I need a JTAG debugger to program it.  Is it possible to use my F1 discover...

Sampling multiple A/D inputs-Quick Question

Posted on February 02, 2013 at 09:18Quick background: I'm using the STM32VL which has 1 ADC peripheral with a possible 18 channels inputs that are multiplexed to the actual ADC. I believe I have the configuration set up correctly for 2 analog inputs...

rj by Associate II
  • 2616 Views
  • 5 replies
  • 0 kudos

SPI 9bit Frame

Posted on January 23, 2013 at 20:08Dear Friends; I use SPI protocol @ stm32f100c4 to interface with GLCD , to interface GLCD frame must be  SPI 9bit. From Datasheet: Stm32f100C4 has two mode 8bit frame or 16 bit frame for sending data by SPI protcol...

Bootloader to Application Transition Not Fully working.

Posted on January 31, 2013 at 19:47I have an application I build from Atollic True Studio that runs correctly stand alone on an STM32F407ZE processor. I am working to insert a boot loader that later branches to the application.  The boot loader runs...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.