2013-02-02 12:45 PM
I has a kit Board STM32F4 Discovery WITH ST-Link / V2 .. I wanted to program/debug another microcontroller STM32F047VGT6 on my personal card .. I have to use the CN2 SWD STM32F4Discovery?? how I should SWD interface connector to microcontroller in my own card ??
Thank you to answer me2013-02-02 2:20 PM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Using%20ST%20Link%20on%20Discovery%20board%20as%20standalone%20ST%20Link&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=23]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fUsing%20ST%20Link%20on%20Discovery%20board%20as%20standalone%20ST%20Link&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FAllItems.aspx¤tviews=23
2013-02-02 2:39 PM
I want to program another microcontroller different than in the kit board ... your solution is to program the microcontroller in this kit board STM32F4Discovery !
2013-02-02 6:06 PM
This is straight forward. You only need two connections plus ground.
At connector CN2: pin 2 - JTCK, connect to target PA14, pin 76 pin 3 - GND, connect to target GND pin 4 - JTMS, connect to target PA13, pin 72 Remove the jumpers at CN3. I don't have my notes here with me so I am going from memory. You will have to wait until Monday for me to double check.2013-02-03 1:11 AM
THANK you for your help .. So I connect the 3-pin directly without reistance or other electronic component .. ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.