STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Final State of PWM

Posted on February 04, 2013 at 10:17 Hi , I am trying to drive a LED Driver IC with a PWM signal on button press. However , it seems that at the end of a PWM cycle the LED final state is not determinable (maybe on/off). It seem that it...

STM32F0 Discovery JP1 (STLINK USART RX,TX)

Posted on February 05, 2013 at 01:35What is the purpose of JP1?  It connects to the STLINK MCU, and via two solder-jumpers on the bottom of the board (SB14,15) to PA9,10 of the 'F051 (the USART-1 pins).  Can the STLINK enumerate as a CDC endpoint, a...

javanzee by Associate
  • 734 Views
  • 0 replies
  • 0 kudos

STM32F051 USART Not working

Posted on February 01, 2013 at 00:39I created some simple code on the STM32F05-Discovery board to write a byte of data repeatedly out USART1.  However when I run this code on my target board the USART doesn't send the data.  The TXE line goes low an...

jprinster by Associate II
  • 1730 Views
  • 5 replies
  • 0 kudos

STM32F103RB SPI latency

Posted on February 04, 2013 at 17:30 Hi all, I trying to use the SPI and I am using uVision Keil. The clock appear with a latency that I can take off by removing while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET); But wh...

0690X000006052fQAA.png
felipe by Associate II
  • 1643 Views
  • 4 replies
  • 0 kudos

Reading ADC Multichannel

Posted on February 04, 2013 at 18:08 I want to read valuefromaccelerometer . Model 1 void GPIO_ADC1_setup() { GPIO_InitTypeDef GPIO_InitStructure; // Enable GPIOC clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA,ENABLE); // Configure PA1 as ...

IAP (In Application Programming) for Flash on STM32F407ZE

Posted on February 04, 2013 at 16:50How long is the bus stalled for program Flash block erase and program operations? I would like to write to and erase Flash sectors while running an application from Flash in sectors not being modified.  Reading ab...

Play mono on stereo channel

Posted on February 04, 2013 at 16:29 Hi , as quoted from the audio implemination of stm32f4 eval : Mono audio streaming is not supported (in order to play mono audio streams, each data should be sent twice < br >on the I2S or should b...

How to drive external flash memory using stm32f103vet6

Posted on February 01, 2013 at 12:10Hi, I have connected external flash memory to my board and using stm32f103vet6 controller. I want to drive this flash memory. So how can i drive that one? And after driving flash memory how can i make sure that fl...

manoj23 by Associate II
  • 2179 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.