STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Embedded World 2013 - Free Discovery Kits

Posted on February 11, 2013 at 09:01Please note that ST will distribute this year again significant number of variety Discovery kits for free during Embedded World show in Nuremberg, February 26-28. For more details and discovery kit registration li...

Ethernet Communication

Posted on February 21, 2013 at 05:52I am using STM32F107rb for ethernet communication. By default in the code it as been set to 10Mbps but i want to change it to 100Mbps so please let me Known where i need to change.... The corresponding code as bee...

aru by Associate II
  • 1805 Views
  • 3 replies
  • 0 kudos

STM32F215VGT split memory problem

Posted on February 21, 2013 at 08:17Hi all, I’m working on a project using CrossWorks IDE Release 2.2.0.2012022100.14129, processor STM32F215VGT and ST-LINK/V2.I'm working on IAP (in application programing) and I needed a place where to put IAP fu...

donev_g by Associate II
  • 2015 Views
  • 4 replies
  • 0 kudos

stm32 USART synchronous Mode

Posted on February 20, 2013 at 11:31 hello I want to use synchronous mode Usart But I'm totally confused When I activate the clock I can not determine if Master or Slave? Please help Me USART_InitTypeDef USART_InitS...

FATFS - slow

Posted on February 20, 2013 at 14:41Hi , A general question about fatfs and SDIO interface , i have a relative many read/seek operations in my program flow,and its taking a segnificant time of the all ''runtime''. Is there anyway to speed things up?...

STM32L Clock Issue

Posted on January 24, 2013 at 08:24Hi all, STM32L processor does not start function with the PLL clock. External Oscillator (HSE) = 8Mhz. PLL clock source (PLLSRC) = HSE PLL multiplication factor (PLLMUL)= 6. PLL Division factor (PLLDIV)= 2. SYSCLK ...

STM32F0 Analog Input

Posted on February 20, 2013 at 15:12Hello, i only got one question: is it possible to connect one external analog input (PA3) to the COMP2 which is used as OPAMP and then use the Output (PA2) directly as input for the ADC and the COMP1?i need to amp...

STM32F4 problem with USART1 INTERRUPT

Posted on February 19, 2013 at 21:52Hi guys,I have a problem with my new schede STM32F407VG. Until now I have been used the STM32F100B so now I'm adapting the code that I wrote. Part of my code is USART with interrupt, so I have wrote a code that re...

External Memory - Hardfault on startup

Posted on February 19, 2013 at 19:27Hi, I am having problem with the external memory. Not so long ago my program used both the internal memory and the external, but I managed to move both the heap and the stack to the external memory (2 megabyte) ,...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.