2013-01-23 11:24 PM
Hi all,
STM32L processor does not start function with the PLL clock. External Oscillator (HSE) = 8Mhz. PLL clock source (PLLSRC) = HSE PLL multiplication factor (PLLMUL)= 6. PLL Division factor (PLLDIV)= 2. SYSCLK source = PLLCLK AHB Prescaler value=1 HCLK = SYSCLK APB1 Prescaler value=1 PCLK1=HCLK APB2 Prescaler value=1 PCLK2=HCLK Can anyone find the problem in clock configuration. Thanks Arul #pll #external-clock2013-01-24 7:06 PM
Ok, but how are you actually programming it? The numbers don't look objectionable, perhaps it's your code. Does the HSE start?
2013-01-24 11:35 PM
> Does the HSE start?
In other words, confirm HSE is working by keeping PLL bypassed first. Do you have a ready made development board, or is this a custom hardware? JW2013-01-24 11:59 PM
Dear clive1,
Thanks for your reply, Now the problem is solved. Reason: Oscillator capacitor component problem,It is working well when i replaced it. Thanks Arul2013-01-25 12:01 AM
Dear waclawek.jan,
Now it is working with the above clock configuration Thanks Arul2013-01-25 12:05 AM
Dear clive and jan,
I have also tested the HSI clock in custom hardware. Without PLL configuration,the processor works well. But when i use HSI with PLL configuration,the processor gets hanged. This is my HSI clock configuration: This is called at systeminit() static void SetSysClockToHSI_PLL(void) { __IO uint32_t StartUpCounter = 0, HSIStatus = 0; /* SYSCLK, HCLK, PCLK2 and PCLK1 configuration ---------------------------*/ /* Enable HSI */ RCC->CR |= ((uint32_t)RCC_CR_HSION); /* Wait till HSI is ready and if Time out is reached exit */ do { HSIStatus = RCC->CR & RCC_CR_HSIRDY; StartUpCounter++; } while((HSIStatus == 0) && (StartUpCounter != HSE_STARTUP_TIMEOUT)); if ((RCC->CR & RCC_CR_HSIRDY) != RESET) { HSIStatus = (uint32_t)0x01; } else { HSIStatus = (uint32_t)0x00; } if (HSIStatus == (uint32_t)0x01) { /* Enable 64-bit access */ FLASH->ACR |= FLASH_ACR_ACC64; /* Enable Prefetch Buffer */ FLASH->ACR |= FLASH_ACR_PRFTEN; /* Flash 1 wait state */ FLASH->ACR |= FLASH_ACR_LATENCY; /* Enable the PWR APB1 Clock */ RCC->APB1ENR |= RCC_APB1ENR_PWREN; /* Select the Voltage Range 1 (1.8V) */ PWR->CR = PWR_CR_VOS_0; /* Wait Until the Voltage Regulator is ready */ while((PWR->CSR & PWR_CSR_VOSF) != RESET) { } /* HCLK = SYSCLK */ RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1; //8Mhz //AHB /* PCLK2 = HCLK */ RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE2_DIV1; // 4Mhz APB2 /* PCLK1 = HCLK */ RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE1_DIV1; //8Mhz //APB1 /* Select HSI as system clock source */ // RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW)); //RCC->CFGR |= (uint32_t)RCC_CFGR_SW_HSI; /* Wait till HSI is used as system clock source */ // while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)0x04) // { // } /* PLL configuration */ RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLMUL | RCC_CFGR_PLLDIV)); RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSI | RCC_CFGR_PLLMUL6 | RCC_CFGR_PLLDIV3); /* Enable PLL */ RCC->CR |= RCC_CR_PLLON; /* Wait till PLL is ready */ while((RCC->CR & RCC_CR_PLLRDY) == 0) { } /* Select PLL as system clock source */ RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW)); RCC->CFGR |= (uint32_t)RCC_CFGR_SW_PLL; /* Wait till PLL is used as system clock source */ while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_PLL) { } } else { /* If HSI fails to start-up, the application will have wrong clock configuration. User can add here some code to deal with this error */ } } Can you find the problem ? Thanks Arul2013-02-20 5:42 AM
Hi Arul,
You can compare your code with the one that you may generate using the System Clock Configuration tool. ST.MCUTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2013-02-20 6:15 AM
/* Select PLL as system clock source */
RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW)); RCC->CFGR |= (uint32_t)RCC_CFGR_SW_PLL; This, after the &=, sets MSI as the clock source, until the |=. I am not sure such rapid switching of clock source is OK. [EDIT] probably yes, as MSI is the default clock source until that moment anyway... [/EDIT] JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.