cancel
Showing results for 
Search instead for 
Did you mean: 

N6 PLL: FRAC change on the fly as in H7 impossible ?

LCE
Principal II

Heyho,

the title says it...

In RM0486, 14.6.5 PLL description, page 437 / 438 I find this:

Using the PLLs in fractional mode

PLL off ... set FRAC ... PLL on

Caution: Do not update DIVN and DIVNFRAC after the PLL has been enabled.

On the other hand, there are comments that some dividers can be changed on the fly.

So maybe it might work? Has anybody tried?

 

With these 4 PLLs and the great clock routing possibilities, the ability to change FRAC values on the fly with this high resolution would be a fantastic feature for synchronization, without using an external VCO.

 

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @LCE 

For  STM32N6, you should not change the FRAC value on the fly. The PLL must be disabled before updating DIVN or DIVNFRAC, as per the official RM0486.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

2 REPLIES 2
FBL
ST Employee

Hi @LCE 

For  STM32N6, you should not change the FRAC value on the fly. The PLL must be disabled before updating DIVN or DIVNFRAC, as per the official RM0486.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
LCE
Principal II

Thanks, would have been a great feature.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.